Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development MicroZed Run sdk application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 364 subscribers
  • Views 1062 views
  • Users 0 members are here
Related

MicroZed Run sdk application

raymadigan
raymadigan over 10 years ago

I bought a MicroZed a long time ago and am finally getting to it.  I have built an application following the Adam Taylor blog to write Hello World to the console.  I have build the application and it seems ok, but I can't get it to run. 

At first I got a message that there was no ARM device on connection local. Cable is not connected to host.

I have created a Target connection to connect to the device:

Type:  Hardware Server
Host:  192.168.1.10
Port: 3121

I get the message that the hardware server is not running on the machine.  I can't find the hardware server to run it.  On some pages I found while googling I found where I was told to run hw_server but that doesn't exist anymore.

What did I miss?  I will work to figure this out, I just need a pointer.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Can you check and see if your host PC is recognizing the HS2 JTAG cable? When you plug the HS2 into your PC USB (even wtihout being connected to the MicroZed) you should hear a 'notification' sound and, in the Windows Device Manager under Universal Serial Bus controllers, you should see a 'USB Serial Converter' added to the list of controllers.

     

    If you disconnect the HS2 from the PC the USB Serial Converter entry should disapear.

     

    If not you might want to go back and install the cable drivers in your Vivado/SDK installation.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • raymadigan
    0 raymadigan over 10 years ago in reply to e14 Contributor

    I am running Linux, ubuntu 14.04.

    I have installed the kernel driver,

    if I lsmod | grep cp210x

    I get
    cp210x    23512  0
    usbserial 45014  2 cp210x, ftdi_sio

    before the board is plugged in
    /dev/ttyUSB0 is present

    when I plug the board in
    /dev/ttyUSB1 is also present.


    if I
    dmesg | grep cp210x  I get
    [  300.683313] usbcore: registered new interface driver cp210x
    [  300.683330] usbserial: USB Serial support registered for cp210x
    [  300.683372] cp210x 8-1:1.0: cp210x converter detected
    [  300.685010] usb 8-1: cp210x converter now attached to ttyUSB1


    I don't know what else to check?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • raymadigan
    0 raymadigan over 10 years ago in reply to e14 Contributor

    I am running Linux, ubuntu 14.04.

    I have installed the kernel driver,

    if I lsmod | grep cp210x

    I get
    cp210x    23512  0
    usbserial 45014  2 cp210x, ftdi_sio

    before the board is plugged in
    /dev/ttyUSB0 is present

    when I plug the board in
    /dev/ttyUSB1 is also present.


    if I
    dmesg | grep cp210x  I get
    [  300.683313] usbcore: registered new interface driver cp210x
    [  300.683330] usbserial: USB Serial support registered for cp210x
    [  300.683372] cp210x 8-1:1.0: cp210x converter detected
    [  300.685010] usb 8-1: cp210x converter now attached to ttyUSB1


    I don't know what else to check?