Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development MicroZed Run sdk application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 364 subscribers
  • Views 1062 views
  • Users 0 members are here
Related

MicroZed Run sdk application

raymadigan
raymadigan over 10 years ago

I bought a MicroZed a long time ago and am finally getting to it.  I have built an application following the Adam Taylor blog to write Hello World to the console.  I have build the application and it seems ok, but I can't get it to run. 

At first I got a message that there was no ARM device on connection local. Cable is not connected to host.

I have created a Target connection to connect to the device:

Type:  Hardware Server
Host:  192.168.1.10
Port: 3121

I get the message that the hardware server is not running on the machine.  I can't find the hardware server to run it.  On some pages I found while googling I found where I was told to run hw_server but that doesn't exist anymore.

What did I miss?  I will work to figure this out, I just need a pointer.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    See if this forum post is helpful:

     

    http://microzed.org/content/usb-uart-problem

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    See if this forum post is helpful:

     

    http://microzed.org/content/usb-uart-problem

     

    -Gary