Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development cannot boot linux on zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 429 views
  • Users 0 members are here
Related

cannot boot linux on zedboard

e14 Contributor
e14 Contributor over 12 years ago

I use u-boot-digilent-2012.04-digilent-13.01.zip and linux-digilent-3.6-digilent-13.01.zip .

I compiled u-boot-digilent-2012.04-digilent-13.01.zip to obtain my own uboot.elf.With my system.bit and fsbl.elf,I creat my BOOT.BIN.Also compile linux-digilent-3.6-digilent-13.01.zip to obtain my own zImage and devicetree.dtb.
and I use official ramdisk8M.image.gz from digilent.

But I cannot boot linux on my zedboard ,the system stopped here(BELOW LOG) , booting the kernel failed.
WHY?whats the problem?

-Boot 2012.04.01 (Mar 19 2014 - 23:52:02)

DRAM:  512 MiB
WARNING: Caches not enabled
MMC:   SDHCI: 0
Using default environment

In:    serial
Out:   serial
Err:   serial
Net:   zynq_gem
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Device: SDHCI
Manufacturer ID: 3
OEM: 5344
Name: SU04G
Tran Speed: 25000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
reading zImage

2461296 bytes read
reading devicetree.dtb

9660 bytes read
reading ramdisk8M.image.gz

3694108 bytes read
## Starting application at 0x00008000 ...
Uncompressing Linux... done, booting the kernel.

it works well with the official BOOT.BIN file.But when using my BOOT.BIN file , it never works .Anyone come aross the same problem ?can you give me some advices?thanks!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Avnet does not provide any support for Digilent Embedded Linux. The Digilent distribution is intended only for students. Please contact your professor or Digilent support at support@digilentinc.com
     
    Please refer to https://github.com/Xilinx for ZedBoard Linux.
     
    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    hi , TroutChaser
    Thanks for your reply !
    Which version of uboot and linux that have tested  ,so I can use it on zedboard ?
    I have download u-boot-xlnx-xilinx-v2013.4.zip and linux-xlnx-xilinx-v2013.4.zip from  https://github.com/Xilinx. But when I boot the linux,it shows Wrong Image Format for bootm command
    ERROR: can't get kernel image!It needs uImage and uramdisk.image.gz ,I have change zImage and ramdisk.image.gz to uImage uramdisk.image.gz. But it shows the same error,I don't know  why .