Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Missing /dev/mpt
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 857 views
  • Users 0 members are here
Related

Missing /dev/mpt

e14 Contributor
e14 Contributor over 10 years ago

I have a target system that has a BOOT.BIN already loaded into its QSPI flash, but when I boot PetaLinux, there is no /dev/mtd.  Doing "cat /proc/mtd" returns no results.  Can I re-create the mtd partitioning from within PetaLinux?  Or is the only solution to load a new BOOT.BIN that was built with the proper MTD settings via Xilinx tools?  And how big does mtd0 need to be for a 7z045?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi,

     

    This was an issue in the 2015.2 release that the factory test resident in the QSPI of some of our boards used (and did not have the fix applied). You can download the BSP for your board from the ZedBoard.org site and you should see the MTD partitions. You don't mention the board you are working with but assuming a Mini-ITX due to the 7z045 question you can find it here:

     

    http://zedboard.org/support/design/2056/17

     

    As for the size of the MTD partitions, it depends on what is going into them. For the boot partition, if the bitstream is included, it has to be big enough to accommodate the 13 MB + size for the 7045. Instructions for changing the partition sizes are in the Boot App note referenced in your other forum thread:

     

    http://zedboard.org/content/split-boot-u-boot-qspi-linux-sd

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi,

     

    This was an issue in the 2015.2 release that the factory test resident in the QSPI of some of our boards used (and did not have the fix applied). You can download the BSP for your board from the ZedBoard.org site and you should see the MTD partitions. You don't mention the board you are working with but assuming a Mini-ITX due to the 7z045 question you can find it here:

     

    http://zedboard.org/support/design/2056/17

     

    As for the size of the MTD partitions, it depends on what is going into them. For the boot partition, if the bitstream is included, it has to be big enough to accommodate the 13 MB + size for the 7045. Instructions for changing the partition sizes are in the Boot App note referenced in your other forum thread:

     

    http://zedboard.org/content/split-boot-u-boot-qspi-linux-sd

     

    -Gary