Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Missing /dev/mpt
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 857 views
  • Users 0 members are here
Related

Missing /dev/mpt

e14 Contributor
e14 Contributor over 10 years ago

I have a target system that has a BOOT.BIN already loaded into its QSPI flash, but when I boot PetaLinux, there is no /dev/mtd.  Doing "cat /proc/mtd" returns no results.  Can I re-create the mtd partitioning from within PetaLinux?  Or is the only solution to load a new BOOT.BIN that was built with the proper MTD settings via Xilinx tools?  And how big does mtd0 need to be for a 7z045?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The problem turned out to be an inconsistency in the hardware description.  If I used an HDF from the full design, an AXI DMA controller was included n the HDF, which caused PetaLinux to attempt to load the DMA driver, and poll one of its registers.  But the bitstream hadn't been loaded, so there was no response.  To fix that, I used an HDF from a dummy design that only included the Zynq PS, but it missed some clocking information that prevented the BOOT.BIN created with it from operating.  So I mixed the BOOT.BIN from the full system with the image.ub from the PS-only system.  It would boot to a linux command prompt, but was not correct.  The missing /dev/mtd was just the most obvious symptom of the inconsistency.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The problem turned out to be an inconsistency in the hardware description.  If I used an HDF from the full design, an AXI DMA controller was included n the HDF, which caused PetaLinux to attempt to load the DMA driver, and poll one of its registers.  But the bitstream hadn't been loaded, so there was no response.  To fix that, I used an HDF from a dummy design that only included the Zynq PS, but it missed some clocking information that prevented the BOOT.BIN created with it from operating.  So I mixed the BOOT.BIN from the full system with the image.ub from the PS-only system.  It would boot to a linux command prompt, but was not correct.  The missing /dev/mtd was just the most obvious symptom of the inconsistency.