Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development how to enable Secure accesses?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 244 views
  • Users 0 members are here
Related

how to enable Secure accesses?

zxj
zxj over 12 years ago



I want to control register ICDISER0,
(address 0xf8f01100, Interrupt Set-enable Register 0).
But it only supports Secure accession.

How can I enable secure mode please?

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    In the Zynq Technical Reference Manual (UG585), right under the definition of the ICDISER register in section 7.3.1, it describes the Write Protection Lock and that it is controlled by writing to the System Level Control register set, SLCR.

     

    Section B.28 of the TRM details the System Level Control Registers and the Write Protection Lock and Unlock functions.

     

    This status is usually set early in the First Stage Boot Loader process. Take a look in the main.c of the default FSBL code for an example of unlocking the SLCR to allow SLCR register writes.

     

    I deleted the duplicate post on this subject. Please do not duplicate questions on the forum.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    In the Zynq Technical Reference Manual (UG585), right under the definition of the ICDISER register in section 7.3.1, it describes the Write Protection Lock and that it is controlled by writing to the System Level Control register set, SLCR.

     

    Section B.28 of the TRM details the System Level Control Registers and the Write Protection Lock and Unlock functions.

     

    This status is usually set early in the First Stage Boot Loader process. Take a look in the main.c of the default FSBL code for an example of unlocking the SLCR to allow SLCR register writes.

     

    I deleted the duplicate post on this subject. Please do not duplicate questions on the forum.

     

    -Gary