Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development U-boot Compiler not executing
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 510 views
  • Users 0 members are here
Related

U-boot Compiler not executing

e14 Contributor
e14 Contributor over 10 years ago

Hai,

    I am using ELDK-4.2 Compiler then now i am executing u-boot commands like make zynq_zc706 same below failures are coming:

 root@caravel:/home/ram/Desktop/uboot-xilinx-v2014.1# make zynq_zc70x_config

/bin/bash: arm-linux-gcc: command not found
/bin/bash: arm-linux-gcc: command not found
dirname: missing operand
Try 'dirname --help' for more information.
Generating include/autoconf.mk
/bin/bash: line 2: arm-linux-gcc: command not found
Generating include/autoconf.mk.dep
/bin/bash: line 2: arm-linux-gcc: command not found

Configuring for zynq_zc70x board...    

Why Eldk not working for ZYNQ Boards With out ELDK compiler which compiler will be using??? 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    Use the gcc compiler that comes with the Xilinx SDK.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • narrucmot
    0 narrucmot over 10 years ago

    The "command not found" error message indicates that perhaps the CROSS_COMPILE environment variable is not set correctly.  Since it appears you are using the ELDK toolchain to build u-boot, you may want to take a look on www.denx.de for support.  The ELDK is their product and they will be best able to support you.  Alternatively, as previously mentioned, you could use the Xilinx SDK.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    I am generated U-Boot.bin file through ELDK.With out fsbl and system.bit this will works or not. In my SD Card only U-Boot.bin file i am putted but it's not working. It is Mandatory or not sir.

    Thanking you,

    Ram.