Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Default hardware description file
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 365 subscribers
  • Views 1688 views
  • Users 0 members are here
Related

Default hardware description file

cascade99
cascade99 over 10 years ago

HI,
Is there any default hardware description file available to download or any document to generate simple .hdf file?
I just like to start my software project which is asking a hardware description file.
Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    If you are using the ZedBoard, MicroZed 7010, ZC702, or the ZC706 board you can select one of the predefined hardware platforms in the SDK.

     

    In the SDK, when you start a 'new application project', use the dropdown box next to 'Hardware Platform' under 'Target Hardware'. If you select one of the pre-defined platforms, such as 'zed_hw_platform (pre-defined)', you will get an hdf file that matches the selected board that you can use with your new software project.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    If you are using the ZedBoard, MicroZed 7010, ZC702, or the ZC706 board you can select one of the predefined hardware platforms in the SDK.

     

    In the SDK, when you start a 'new application project', use the dropdown box next to 'Hardware Platform' under 'Target Hardware'. If you select one of the pre-defined platforms, such as 'zed_hw_platform (pre-defined)', you will get an hdf file that matches the selected board that you can use with your new software project.

     

    -Gary