Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Default hardware description file
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 365 subscribers
  • Views 1688 views
  • Users 0 members are here
Related

Default hardware description file

cascade99
cascade99 over 10 years ago

HI,
Is there any default hardware description file available to download or any document to generate simple .hdf file?
I just like to start my software project which is asking a hardware description file.
Thanks

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 10 years ago

    There is no default hardware description file because there is no default hardware. What hardware are you targeting? There is likely a solution containing an HDF that you could start with.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cascade99
    0 cascade99 over 10 years ago in reply to bhfletcher

    I have zedboard eval board, I followed the petalinux "Workflow Tutorial"(UG1156), page 7, "petalinux-build", I got the following err:
    [INFO ] install linux/kernel
    [ERROR] ERROR: Invalid ELF file '/opt/PetaLinux/project/Avnet-Digilent-ZedBoard-2015.4/images/linux/vmlinux'
    [ERROR] make[1]: *** [package-subsystem-FIT] Error 255
    ERROR: Failed to build linux

    I'm using newest release 2015.4, any comments? Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chenzhenyuch
    0 chenzhenyuch over 9 years ago in reply to cascade99

    I have also met the similar issue,following is the message: 

    [INFO ] vmlinux linux/kernel
    [INFO ] install linux/kernel
    [INFO ] package zImage
    [INFO ] zImage linux/kernel
    [INFO ] install linux/kernel
    [ERROR] ERROR: Invalid ELF file '/home/z/user/project_test/images/linux/vmlinux'
    [ERROR] make[1]: *** [package-subsystem-FIT] Error 255
     
    Maybe it is not the fault of HDF file because I have tried more than one HDF file and met the same issue as above.
     
    It seems that  the package of openssl-devel.x86_64 and  openssl098e.x86_64 need to be re-installed. You can refer "http://www.gkaindia.com/failed-when-build-petalinux/" for details. 
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • chenzhenyuch
    0 chenzhenyuch over 9 years ago in reply to cascade99

    I have also met the similar issue,following is the message: 

    [INFO ] vmlinux linux/kernel
    [INFO ] install linux/kernel
    [INFO ] package zImage
    [INFO ] zImage linux/kernel
    [INFO ] install linux/kernel
    [ERROR] ERROR: Invalid ELF file '/home/z/user/project_test/images/linux/vmlinux'
    [ERROR] make[1]: *** [package-subsystem-FIT] Error 255
     
    Maybe it is not the fault of HDF file because I have tried more than one HDF file and met the same issue as above.
     
    It seems that  the package of openssl-devel.x86_64 and  openssl098e.x86_64 need to be re-installed. You can refer "http://www.gkaindia.com/failed-when-build-petalinux/" for details.