Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development spi example
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 939 views
  • Users 0 members are here
Related

spi example

starbright
starbright over 11 years ago

Does someone has got a small example about howto communicate via SPI to a device? What is to do?

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    Can you be a bit more specific? Is this for Zynq? If so, are you trying to use a PS or a PL peripheral? Is there a particular piece of hardware that you are targeting?

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • starbright
    0 starbright over 11 years ago

    Yep it is for the MicroZed, accessing from PS (Linux) an external chip. This can be for instance an temperature sensor with SPI interface. A generic approach would be best, so that I can access all kind of SPI devices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago in reply to starbright

    Some of our partners provide Pmods with devices that you can easily connect to Avnet boards. One partner is Maxim. Take a look at the MAX31723PMB1# Pmod -- http://www.maximintegrated.com/en/products/analog/sensors-and-sensor-interface/MAX31723PMB1.html

     

    It's a SPI-based temperature sensor. They have support for ZedBoard, but hopefully it's not too difficult to port over to MicroZed. Do you have an FMC or IO Carrier to give access to the PL I/Os?

     

    Click on the Design Resources tab to find the designs.

    http://www.maximintegrated.com/en/products/analog/sensors-and-sensor-interface/MAX31723PMB1.html/tb_tab2#tab2

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • starbright
    0 starbright over 11 years ago

    Thank for this links - idea is good. But this is for ISE and rather complex stuff. I do have a MicroZed I/O Carrier board.

    I think, the simpliest way is use a spidev driver, as there is already an example in kernel.

    So I included SPIDEV into kernel configuration. Nevertheless there is no /dev/spi* device to see. I checked the devicetree. In the section
    tps7_axi_interconnect_0: amba@0 {
    there are two spi nodes:
    ttps7_spi_0: ps7-spi@e0006000 {
    tttclock-names = "ref_clk", "pclk", "aper_clk";
    tttclocks = <&clkc 25>, <&clkc 34>, <&clkc 34>;
    tttcompatible = "xlnx,zynq-spi-r1p6", "xlnx,ps7-spi-1.00.a";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = <0 26 4>;
    tttnum-chip-select = <4>;
    tttreg = <0xe0006000 0x1000>;
    ttt#address-cells = <1>;
    ttt#size-cells = <0>;
    tt} ;
    ttps7_spi_1: ps7-spi@e0007000 {
    tttclock-names = "ref_clk", "pclk", "aper_clk";
    tttclocks = <&clkc 26>, <&clkc 35>, <&clkc 35>;
    tttcompatible = "xlnx,zynq-spi-r1p6", "xlnx,ps7-spi-1.00.a";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = <0 49 4>;
    tttnum-chip-select = <4>;
    tttreg = <0xe0007000 0x1000>;
    ttt#address-cells = <1>;
    ttt#size-cells = <0>;
    tt} ;

    But this seems to be not enough to get an spi device running.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    I found a few discussions that might be helpful:

    https://forums.xilinx.com/t5/Embedded-Linux/How-to-use-XPS-SPI-core-driver-in-linux/td-p/73313

    https://forums.xilinx.com/t5/Embedded-Linux/linux-SPI-for-zynq/td-p/417133

    http://www.wiki.xilinx.com/Linux+SPI+Driver

     

    Bryan