Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PS EMIO SFP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 690 views
  • Users 0 members are here
Related

PS EMIO SFP

e14 Contributor
e14 Contributor over 9 years ago

MAC0 with PHY MARVELL, MAC1 and the PL XILINX PHY  are recognize at the boot of petalinux as follow:

macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 146 (00:0a:35:00:1e:53)
macb e000b000.ethernet eth0: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=e000b000.etherne:00, irq=-1)

macb e000c000.ethernet eth1: Cadence GEM rev 0x00020118 at 0xe000c000 irq 147 (f6:d5:bb:ce:5e:1f)
macb e000c000.ethernet eth1: attached PHY driver [Xilinx PCS/PMA PHY] (mii_bus:phy_addr=e000c000.etherne:00, irq=-1)

But link status don't go up for Ethernet 1 and only Ethernet0 is valid after auto negotiation as shown with the following messages given by petalinux boot:  
Configuring network interfaces... udhcpc (v1.23.1) started
Sending discover...
Sending discover...
macb e000b000.ethernet eth0: link up (1000/Full)
Sending discover...
No lease, forking to background
The connectivity between MAC1 and 1G/2G Ethernet PCS/PMA is based on XAPP1082 ps_emio_sfp script.
Does someone test this configuration on the mmp board?
(and solve also that kind of problem)
 
Thanks

PS: I use a SFPC1110 transceiver module plugged in the SFP connector on the Base Board

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Fredb,

    The IP core being used is from Xilinx, so I am going to suggest that they are best fit to answer your question. I also see that you have already contacted them. Best of luck.

    Xilinx Post : https://forums.xilinx.com/t5/Embedded-Linux/XAPP1082-PS-EMIO-SFP/m-p/743223#M18109

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Fredb,

    The IP core being used is from Xilinx, so I am going to suggest that they are best fit to answer your question. I also see that you have already contacted them. Best of luck.

    Xilinx Post : https://forums.xilinx.com/t5/Embedded-Linux/XAPP1082-PS-EMIO-SFP/m-p/743223#M18109

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer