Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development No option to create PetaLinux BSP on XSDK
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 365 subscribers
  • Views 2656 views
  • Users 0 members are here
Related

No option to create PetaLinux BSP on XSDK

y_okada
y_okada over 11 years ago

I am trying to create custom PetaLinux BSP on XSDK.

I made .hdf file using Vivado. Then, on XSDK, I selected to create BSP importing the hdf file. However, on the windows with title "New Board Support Package Project", on "Board Support Package OS" selection, I only see "standalone" not "PetaLinux".

Is this because I am using XSDK installed on Windows?

If I install the XSDK on Linux, can I select "PetaLinux" on the "Board Support Package OS"?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I'm also trying to configure xsdk with the linux bsp, but 2014.4 has the same edk_user_repository structure as described by y_okada. Namely that the only two folders under edk_user_repository in Petalinux 2014.2 are:
      device-tree-generator
      sw_apps

    Note that there is no petalinux entry in the edk repo.

    Xilinx: Is this repo available in Petalinux 2014.4 to allow creation of a project with a linux BSP in XSDK? If so, where can it be found?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I'm also trying to configure xsdk with the linux bsp, but 2014.4 has the same edk_user_repository structure as described by y_okada. Namely that the only two folders under edk_user_repository in Petalinux 2014.2 are:
      device-tree-generator
      sw_apps

    Note that there is no petalinux entry in the edk repo.

    Xilinx: Is this repo available in Petalinux 2014.4 to allow creation of a project with a linux BSP in XSDK? If so, where can it be found?