Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Problems with .dts while booting Linux on custom hardware
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 494 views
  • Users 0 members are here
Related

Problems with .dts while booting Linux on custom hardware

e14 Contributor
e14 Contributor over 12 years ago

Hello everyone!

I have a question on Linux.
After I succeeded booting Linux on ADV7511 Reference Design on my Zedboard I created custom Reference Design with only I2C and SPI outputs from the PS. It has no devices in the PL connected to the PS.
I've done everything like usual:
.bit - file in Vivado;
fsbl - file in SDK;
u-boot - like it is told in Analog Devices tutorial.
I have also managed to compile uImage and develop a custom .dts for my hardware.
So now it reads u-boot o'k, but while starting kernel I get this error:
-----------------------------------------------------------------------
Starting kernel ...

Error: unrecognized/unsupported device tree compatible list:
[ 'xlnx,zynq-7000' ]

Available machine support:


ID (hex)        NAME
ffffffff        ARM-Versatile Express
000008e0        ARM-Versatile Express
00000d32        Xilinx Zynq Platform


Please check your kernel config and/or bootloader.
-----------------------------------------------------------------------
I've already tried changing the compatible parameter to "xlnx,zynq-zed" and it worked in the same way. And I've also tried to change it to "xlnx,zynq-zc702" just in case, but in couldn't find a clock source.
Can anyone help me?

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 12 years ago

    Hi resalmon,

    Can you please elaborate on which instructions you are following for the "Linux on ADV7511 Reference Design"?

    Are you referring to the instructions from ADI seen here?

    http://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq

    If so, I assume that you checked out the xcomm_zynq branch and configured your Linux kernel with the zynq_xcomm_adv7511_defconfig.

    In that case, it should be okay to use the following compatibility string in your devicetree:

    compatible = "xlnx,zynq-zc702";

    If you are getting an error message about a clock source when you use that compatibility string, can you please post some more information such as error messages so that we can understand the error better?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Yes, I tried that string and it worked. Actually, the problem was solved two weeks ago. Thank you for your reply.