Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development GPIO controllers_Kernel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 344 views
  • Users 0 members are here
Related

GPIO controllers_Kernel

e14 Contributor
e14 Contributor over 10 years ago

Hi,

Im booting Linux on a Microzed 7010

I tried to see which gpio controlles are available so i did /sys/kernel/debug/gpio but when accessing the kernel i only see:

fscaps   notes                           uevent_helper

mm       rcu_expidited             uevent_segnum
 
any help??

  • Sign in to reply
  • Cancel
  • narrucmot
    0 narrucmot over 10 years ago

    What Linux are you booting?  PetaLinux?

    Take a look in /sys/class/gpio.  You should see your gpio peripheral(s) there, e.g. named gpiochip0, etc.  If you don't see any gpiochip<n> devices listed, but expect to see them, you likely have a mismatch between your hardware platform (Zynq PL bitstream) and Linux devicetree.  You can follow the instructions here to manually exercise the GPIO bits (read switches, toggle LEDs, etc.):

    http://www.wiki.xilinx.com/Linux+GPIO+Driver

    If you are booting PetaLinux you can use the provided gpio-demo application to exercise the GPIO bits using the steps below:

    1.   If you haven’t already, login to PetaLinux using the provided credentials.
    1.   Identify the location of the GPIO peripherals.  Enter the following command to print the kernel boot and diagnostic messages and pipe the output through a grep filter to locate the GPIO peripherals in the system:

    # dmesg |grep gpio

    1.   You many experiment with the gpio-demo application to turn on the LEDs and read the switches.  Enter the following command to turn on an LED:

    # gpio-demo -g <gpio base> -o 0x1

    1.   Use the application to read the DIP and PB switches.

    # gpio-demo -g <gpio base> –i