Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Xapp1026 bsp generation problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 360 views
  • Users 0 members are here
Related

Xapp1026 bsp generation problem

e14 Contributor
e14 Contributor over 10 years ago

I have done the Xapp1026 example  which is based on Freertos ,  and was working fine in hardware and software
I have done a modification on the hardware design by adding XADC and this also worked fine  and the BSP was regenerated perfectly based on that, and then I modified the hardware design again to add DMA engine, but then the BSP generation ends up with errors because the xil_types.h generated in the BSP is earlier version

Ver   Who    Date   Changes
* ----- ---- -------- -------------------------------------------------------
* 1.00a hbm  07/14/09 First release
* 3.03a sdm  05/30/11 Added Xuint64 typedef and XUINT64_MSW/XUINT64_LSW macros


which is not supported by dma driver axidma_v9_0

while this version of xil_types.h is needed
Ver   Who    Date   Changes
* ----- ---- -------- -------------------------------------------------------
* 1.00a hbm  07/14/09 First release
* 3.03a sdm  05/30/11 Added Xuint64 typedef and XUINT64_MSW/XUINT64_LSW macros
* 5.00 tpkp  05/29/14 Made changes for 64 bit architecture
*tsrt  07/14/14 Use standard definitions from stdint.h and stddef.h
*tt      Define LONG and ULONG datatypes and mask values


everytime I try to replace the file or modify it , its getting replaced by the earlier version at the next build

so anyone  have met similar problems and how to get over it

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Maged,

    It looks like some FreeRTOS users have found a workaround for the issue here:

     

    http://interactive.freertos.org/entries/82522745-FreeRTOS-LWIP-for-Vivado-2015-1

     

    -Gary