Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development User app not packaged in SD card boot image
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 364 subscribers
  • Views 1827 views
  • Users 0 members are here
Related

User app not packaged in SD card boot image

vishal.bh30
vishal.bh30 over 8 years ago

Hello,

 

I am following UG1144 and 1157 documentation on petalinux from Xilinx for ultrazed board. i have Vivado 2017.3 and petalinux 2017.3 installed in Unbuntu 16.04 64 bit machine.

 

the issue is 

when i create the package and load the - BOOT.bin and image.ub  file on the SD card and load it on the board, i am not able to see myapp inside /usr/bin folder .. but if i look into the rootfs.tar.gz file  ?(which is a tarball or the filesystem, i can see the myapp in /usr/bin path ) ? not sure what is wrong here .. is board getting booted correctly ?

 i have tried to explain my issue in detail here:

https://forums.xilinx.com/t5/Embedded-Linux/How-to-include-a-user-app-in-petalinux-SD-Card-package/td-p/824969

 

I hope someone from Avnet would be able to look into this.. need to resolve this issue 

  • Sign in to reply
  • Cancel

Top Replies

  • zedhed
    zedhed over 8 years ago +1
    Hi vishal.bh30, I see from the Xilinx forum that you have verified that you are loading BOOT.BIN from the SD card so that is a good first step for troubleshooting. I suspect that you may be booting the…
Parents
  • vishal.bh30
    0 vishal.bh30 over 8 years ago

    Hello,

    So i was able to find that this is a kown issue with Xilinx : https://www.xilinx.com/support/answers/69780.html

    But when i applied this fix .. i am now getting a different error :

    PLL: shutdown

    Found that this was another issue : https://www.xilinx.com/support/answers/69764.html

    and applied its given fix in Vivado and regenerated the bitstream and imported it the project but then got this error:

    VFS: cannot open root device "mmcblk0p2" or unknown-block(179,2) : error -6

    Kernel panic  VFS : Unable to mount root fs on unknown-block(179,2)

    following what was discussed here : https://forums.xilinx.com/t5/Embedded-Development-Tools/Beginners-problems-with-Ultrazed-eg/td-p/800802

    I tried updating the system-user.dtsi file under : petalinux_prj/proj-spec/meta-user/recipes-bsp/device-tree/files/system-user.dtsi,

    but now i keep getting error :

    * Unable to read file system.dtb *

    Also i was able to generate the project from avnet scripts on github... li tried to copy the same system-user.dtsi file in my folder and yocto started to give build errors....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vishal.bh30
    0 vishal.bh30 over 8 years ago in reply to vishal.bh30
    having the following when i execute petalinux-config command :
     
    Go to Subsystem AUTO Hardware Settings -> Advanced bootable images storage Settings -> boot image settings and set ‘image storage media’ option to ‘primary sd’
    Go to Subsystem AUTO Hardware Settings -> Advanced bootable images storage Settings -> kernel image settings and set ‘image storage media’ option to ‘primary sd’
    Go to Subsystem AUTO Hardware Settings -> Advanced bootable images storage Settings -> dtb image settings and set ‘image storage media’ option to ‘primary sd’
    Go to Image Packaging Configurations and set ‘Root filesystem type’ option to ‘SD card’
     
    source : https://medium.com/developments-and-implementations-on-zynq-7000-ap/install-ubuntu-16-04-lts-on-zynq-zc702-using-petalinux-2016-4-e1da902eaff7
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vishal.bh30
    0 vishal.bh30 over 8 years ago in reply to vishal.bh30
    having the following when i execute petalinux-config command :
     
    Go to Subsystem AUTO Hardware Settings -> Advanced bootable images storage Settings -> boot image settings and set ‘image storage media’ option to ‘primary sd’
    Go to Subsystem AUTO Hardware Settings -> Advanced bootable images storage Settings -> kernel image settings and set ‘image storage media’ option to ‘primary sd’
    Go to Subsystem AUTO Hardware Settings -> Advanced bootable images storage Settings -> dtb image settings and set ‘image storage media’ option to ‘primary sd’
    Go to Image Packaging Configurations and set ‘Root filesystem type’ option to ‘SD card’
     
    source : https://medium.com/developments-and-implementations-on-zynq-7000-ap/install-ubuntu-16-04-lts-on-zynq-zc702-using-petalinux-2016-4-e1da902eaff7