Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zedboard: Enable PL Interrupt in FreeRTOS
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 2664 views
  • Users 0 members are here
Related

Zedboard: Enable PL Interrupt in FreeRTOS

ddervaric
ddervaric over 9 years ago

Hi,

 

I'm quite new to Application Development for Zynq Chips.

I successfully implemented a PL->PS interrupt in a baremetal environment using the tutorials. Now I thought porting it to FreeRTOS would be straight forward but once the task scheduler runs I can't get any interrupt fired.

I'm sure I'll just have to link my ISR to some FreeRTOS Task/function but can't find any hints on how to do so. I would really appreciate it if someone could point me in the right direction.

Edit: I'm using an AXI GPIO Core connected to the push buttons with F2PIRQ. The GPIO is initialized using the XGpio_* functions.

My initializing code is the following (called from main, as any call from a task will crash the system):

 

int SetupInterruptSystem()
{
    int Result;
    INTC *IntcInstancePtr = &Intc;

    XScuGic_Config *IntcConfig;

    /*
     * Initialize the interrupt controller driver so that it is ready to
     * use.
     */
    IntcConfig = XScuGic_LookupConfig(INTC_DEVICE_ID);
    if (NULL == IntcConfig) {
        return XST_FAILURE;
    }


    Result = XScuGic_CfgInitialize(IntcInstancePtr, IntcConfig,
                    IntcConfig->CpuBaseAddress);
    if (Result != XST_SUCCESS) {
        return XST_FAILURE;
    }


    Xil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_INT,
             (Xil_ExceptionHandler)INTC_HANDLER, IntcInstancePtr);

    /* Enable non-critical exceptions */
    Xil_ExceptionEnable();


    /*
     * Connect the interrupt handler that will be called when an
     * interrupt occurs for the device.
     */
    Result = XScuGic_Connect(IntcInstancePtr, XPAR_FABRIC_AXI_BTN_IN_IP2INTC_IRPT_INTR,
                 (Xil_ExceptionHandler)GpioIsr, (void *) &Gpio);
    if (Result != XST_SUCCESS) {
        return Result;
    }

    XGpio_InterruptEnable(&Gpio, 1);
    XGpio_InterruptGlobalEnable(&Gpio);

    XScuGic_Enable(IntcInstancePtr, XPAR_FABRIC_AXI_BTN_IN_IP2INTC_IRPT_INTR);

    /*
     * Initialize the exception table and register the interrupt
     * controller handler with the exception table
     */
    //Xil_ExceptionInit();


    return XST_SUCCESS;
}

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello ddervaric,

    Please take a look at this post.

    https://forums.xilinx.com/t5/Embedded-Development-Tools/PL-PS-Interrupt-for-Zynq-running-FreeRTOS/td-p/487570

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello ddervaric,

    Please take a look at this post.

    https://forums.xilinx.com/t5/Embedded-Development-Tools/PL-PS-Interrupt-for-Zynq-running-FreeRTOS/td-p/487570

    Thanks,

    Josh