Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Standalone Baremetal Write/Read to SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 1330 views
  • Users 0 members are here
Related

Standalone Baremetal Write/Read to SD card

e14 Contributor
e14 Contributor over 10 years ago

Hi all,

I am trying to write/read to an SD card using a baremetal application.  I DO NOT want to format it as FAT32.  I simply want to do the simplest bare read/write possible.  I am using the Zynq 7Z02.

I've tracked it down to failing within the "readpolled" function call (a function in the xsdps.c file).  Within that file, it fails somewhere in here because apparently StatusReg & XSDPS_INTR_ERR_MASK == 1 (aka, read has failed):

do {
StatusReg = XSdPs_ReadReg16(InstancePtr-Config.BaseAddress,
tXSDPS_NORM_INTR_STS_OFFSET);
if (StatusReg & XSDPS_INTR_ERR_MASK) {
t/*
t * Write to clear error bits
t */
tXSdPs_WriteReg16(InstancePtr->Config.BaseAddress,
tttXSDPS_ERR_INTR_STS_OFFSET,
tttXSDPS_ERROR_INTR_ALL_MASK);
tStatus = XST_FAILURE;
tgoto RETURN_PATH;
t}
} while((StatusReg & XSDPS_INTR_TC_MASK) == 0);


I hope someone can help.  Below you'll find the code which initializes the SD card.
This is what I have so far:

uint8_t tSCR[8] __attribute__ ((aligned(32)));
uint8_t tReadBuff[64] __attribute__ ((aligned(32)));

XSdPs_Config *SdConfig;

int statusSdFlash = 0;
int readSd = 0;

// Check if card is in the socket

uint32_t StatusReg = XSdPs_GetPresentStatusReg(XPAR_XSDPS_0_BASEADDR);

if ((StatusReg & XSDPS_PSR_CARD_INSRT_MASK) == 0){
  return 1;tt// No disk
}

//Initialize the host controller

SdConfig = XSdPs_LookupConfig(XPAR_PS7_SD_0_DEVICE_ID);
tif (NULL == SdConfig){
ttreturn 1;
t}

statusSdFlash = XSdPs_CfgInitialize(&sd0Inst, SdConfig, SdConfig->BaseAddress);
t
if (statusSdFlash != XST_SUCCESS){
ttreturn 1;
t}

statusSdFlash = XSdPs_SdCardInitialize(&sd0Inst);
if (statusSdFlash != XST_SUCCESS){
treturn 1;
t}

statusSdFlash = XSdPs_Change_ClkFreq(&sd0Inst, 25000000/*XPAR_PS7_SD_0_SDIO_CLK_FREQ_HZ*/);
tif (statusSdFlash != XST_SUCCESS){
ttreturn 1;
t}

statusSdFlash = XSdPs_Select_Card(&sd0Inst);
tif (statusSdFlash != XST_SUCCESS){
ttreturn 1;
t}

statusSdFlash = XSdPs_Get_BusWidth(&sd0Inst, SCR);
tif (statusSdFlash != XST_SUCCESS){
ttreturn 1;
t}

statusSdFlash = XSdPs_Get_BusSpeed(&sd0Inst, ReadBuff);
tif (statusSdFlash != XST_SUCCESS){
ttreturn 1;
t}

if(ReadBuff[13] & HIGH_SPEED_SUPPORT){
tstatusSdFlash = XSdPs_Change_BusSpeed(&sd0Inst);
ttif (statusSdFlash != XST_SUCCESS){
tttreturn 1;
tt}
t}

statusSdFlash = XSdPs_Pullup(&sd0Inst);
tif (statusSdFlash != XST_SUCCESS){
ttreturn 1;
t}

if (SCR[1] & WIDTH_4_BIT_SUPPORT){
tstatusSdFlash = XSdPs_Change_BusWidth(&sd0Inst);
ttif (statusSdFlash != XST_SUCCESS){
tttreturn 1;
tt}
t}

statusSdFlash = XSdPs_SetBlkSize(&sd0Inst, XSDPS_BLK_SIZE_512_MASK);
tif (statusSdFlash != XST_SUCCESS){
ttreturn 1;
t}

statusSdFlash = XSdPs_ReadPolled(&sd0Inst, 1, 1, sdBuf);

tif (statusSdFlash != XST_SUCCESS){
ttreturn 1;
t}
}

//separate function
XSdPs_Config *XSdPs_LookupConfig(uint16_t DeviceId){

tXSdPs_Config *CfgPtr = NULL;
tint Index;

tXSdPs_Config XSdPs_ConfigTable[] =
t{
tt{
ttXPAR_XSDPS_0_DEVICE_ID,
ttXPAR_XSDPS_0_BASEADDR,
ttXPAR_XSDPS_0_SDIO_CLK_FREQ_HZ
tt}
t};
t
for (Index = 0; Index < XPAR_XSDPS_NUM_INSTANCES; Index++) {

if (XSdPs_ConfigTable[Index].DeviceId == DeviceId) {
tCfgPtr = &XSdPs_ConfigTable[Index];
tbreak;
t}
}
return CfgPtr;
}

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    As mentioned earlier you may need to check with Xilinx on ZC702 specific requirements. This AR refers you to Chapter 25 of the Zynq TRM, UG585: http://www.xilinx.com/support/answers/59476.html

     

    The easiest way to verify that your hardware is right would be to export your hardware build to the SDK and implement some known good applications that use the SD Card. Generate an SD bootable image and see if it works. Find some example or reference design for the ZC702 that read and writes the SD Card and make sure it works on your hardware.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    As mentioned earlier you may need to check with Xilinx on ZC702 specific requirements. This AR refers you to Chapter 25 of the Zynq TRM, UG585: http://www.xilinx.com/support/answers/59476.html

     

    The easiest way to verify that your hardware is right would be to export your hardware build to the SDK and implement some known good applications that use the SD Card. Generate an SD bootable image and see if it works. Find some example or reference design for the ZC702 that read and writes the SD Card and make sure it works on your hardware.

     

    -Gary