Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development linux kernel 3.6 stop at bio: create slab <bio-0> at 0  under EDK 14.4 tools
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 362 subscribers
  • Views 208 views
  • Users 0 members are here
Related

linux kernel 3.6 stop at bio: create slab <bio-0> at 0  under EDK 14.4 tools

e14 Contributor
e14 Contributor over 13 years ago

I have compiled the ADI kernel, building the "xcomm_zynq" branch from "git://github.com/analogdevicesinc/linux.git"

When attempting to boot this kernel under EDK 14.3 tools, It can start successly, but when moving my project to EDK 14.4, I get the following output, and it hangs or crashes, please help:

U-Boot 2011.03 (Mar 13 2013 - 19:33:12)                                       

DRAM:  512 MiB
MMC:   SDHCI: 0
Using default environment

In:    serial
Out:   serial
Err:   serial
Net:   zynq_gem
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Device: SDHCI                                                                                                                      
Manufacturer ID: 1b                                                                                                                
OEM: 534d                                                                                                                          
Name: 00000                                                                                                                        
Tran Speed: 25000000                                                                                                               
Rd Block Len: 512                                                                                                                  
SD version 1.10                                                                                                                    
High Capacity: Yes                                                                                                                 
Capacity: 8068792320                                                                                                               
Bus Width: 1-bit                                                                                                                   
reading zImage                                                                                                                     
                                                                                                                                   
2810416 bytes read                                                                                                                 
reading devicetree.dtb                                                                                                             
                                                                                                                                   
4370 bytes read                                                                                                                    
reading ramdisk8M.image.gz                                                                                                         
                                                                                                                                   
3694108 bytes read                                                                                                                 
## Starting application at 0x00008000 ...                                                                                          
Uncompressing Linux... done, booting the kernel.                                                                                   
Booting Linux on physical CPU 0                                                                                                    
Linux version 3.6.0-g0ac8650-dirty (wzb@stepzhibin) (gcc version 4.6.3 (Sourcery CodeBench Lite 2012.03-83) ) #1 SMP PREEMPT Wed Ma3
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d                                                                    
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache                                                           
Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZED                                                                              
bootconsole [earlycon0] enabled                                                                                                    
INITRD: 0x00800000+0x00800000 overlaps in-use memory region - disabling initrd                                                     
cma: CMA: reserved 40 MiB at 1d800000                                                                                              
Memory policy: ECC disabled, Data cache writealloc                                                                                 
PERCPU: Embedded 7 pages/cpu @c0e56000 s7872 r8192 d12608 u32768                                                                   
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048                                                        
Kernel command line: console=ttyPS0,115200 root=/dev/ram rw initrd=0x800000,8M earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=0
PID hash table entries: 2048 (order: 1, 8192 bytes)                                                                                
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)                                                                    
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)                                                                     
Memory: 512MB = 512MB total                                                                                                        
Memory: 468072k/468072k available, 56216k reserved, 0K highmem                                                                     
Virtual kernel memory layout:                                                                                                      
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)                                                                                  
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)                                                                                  
    vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)                                                                                  
    lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)                                                                                  
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)                                                                                  
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)                                                                                  
      .text : 0xc0008000 - 0xc04ccf6c   (4884 kB)                                                                                  
      .init : 0xc04cd000 - 0xc04f3ec0   ( 156 kB)                                                                                  
      .data : 0xc04f4000 - 0xc0544900   ( 323 kB)                                                                                  
       .bss : 0xc0544924 - 0xc0a4c250   (5151 kB)                                                                                  
Preemptible hierarchical RCU implementation.                                                                                       
        RCU lockdep checking is enabled.                                                                                           
        Dump stacks of tasks blocking RCU-preempt GP.                                                                              
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.                                                                       
NR_IRQS:512                                                                                                                        
Zynq clock init                                                                                                                    
xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43                                                                                       
------------[ cut here ]------------                                                                                               
WARNING: at arch/arm/kernel/smp_twd.c:389 time_init+0x20/0x30()                                                                    
twd_local_timer_of_register failed (-19)                                                                                           
Modules linked in:                                                                                                                 
[<c001331c>] (unwind_backtrace+0x0/0xe0) from [<c001f894>] (warn_slowpath_common+0x4c/0x64)                                        
[<c001f894>] (warn_slowpath_common+0x4c/0x64) from [<c001f92c>] (warn_slowpath_fmt+0x2c/0x3c)                                      
[<c001f92c>] (warn_slowpath_fmt+0x2c/0x3c) from [<c04d0eb0>] (time_init+0x20/0x30)                                                 
[<c04d0eb0>] (time_init+0x20/0x30) from [<c04cd6a0>] (start_kernel+0x1b8/0x2fc)                                                    
[<c04cd6a0>] (start_kernel+0x1b8/0x2fc) from [<00008044>] (0x8044)                                                                 
---[ end trace 1b75b31a2719ed1c ]---                                                                                               
sched_clock: 32 bits at 100 Hz, resolution 10000000ns, wraps every 4294967286ms                                                    
Console: colour dummy device 80x30                                                                                                 
Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar                                                           
... MAX_LOCKDEP_SUBCLASSES:  8                                                                                                     
... MAX_LOCK_DEPTH:          48                                                                                                    
... MAX_LOCKDEP_KEYS:        8191                                                                                                  
... CLASSHASH_SIZE:          4096                                                                                                  
... MAX_LOCKDEP_ENTRIES:     16384                                                                                                 
... MAX_LOCKDEP_CHAINS:      32768                                                                                                 
... CHAINHASH_SIZE:          16384                                                                                                 
memory used by lock dependency info: 3695 kB                                                                                      
per task-struct memory footprint: 1152 bytes                                                                                      
Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)                                                                           
pid_max: default: 32768 minimum: 301                                                                                               
Mount-cache hash table entries: 512                                                                                                
CPU: Testing write buffer coherency: ok                                                                                            
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000                                                                                   
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available                                                       
Setting up static identity map for 0x3645a8 - 0x3645dc                                                                             
Map SLCR registers                                                                                                                 
CPU1: Booted secondary processor                                                                                                   
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001                                                                                   
Brought up 2 CPUs                                                                                                                  
SMP: Total of 2 processors activated (2664.03 BogoMIPS).                                                                           
devtmpfs: initialized                                                                                                              
NET: Registered protocol family 16                                                                                                 
DMA: preallocated 256 KiB pool for atomic coherent allocations                                                                     
xgpiops e000a000.gpio: gpio at 0xe000a000 mapped to 0xe0806000                                                                     
registering platform device 'pl330' id 0                                                                                           
registering platform device 'arm-pmu' id 0                                                                                         
registering platform device 'zynq-dvfs' id 0                                                                                       
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.                                                        
hw-breakpoint: maximum watchpoint size is 4 bytes.                                                                                 
MIO pin 11 not assigned(00001760)                                                                                                  
xslcr xslcr.0: at 0xF8000000 mapped to 0xF8000000                                                                                  
bio: create slab <bio-0> at 0