Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development can't run app on board with ubuntu file system
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 353 views
  • Users 0 members are here
Related

can't run app on board with ubuntu file system

e14 Contributor
e14 Contributor over 12 years ago

Hi,
I cross-compiled an ELF and uploaded it into rootfs(Ubuntu12.10), but not able to run it on board. The console printout:"-bash: ./filename: No such file or directory."
Tried chmod, but no help.
The ELF can be run on board with the origin file system (deriving from uramdisk.image.gz)
Any idea?
thank you !

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    There are several reasons why this might happen, but I think the most likely cause is that the executable you are trying run is either compiled for the wrong word length, or there are dynamic libraries the executable requires that are not installed on the Ubuntu target.  You can check the file format by going to the directory on your target that contains your executable, and type:   file <executable name>.   You should get something back that indicates it is a 32-bit LSB executable for ARM if it is the correct format, in which case it likely will also tell you that it is dynamically linked.   If the latter is the case, then of course the solution is to install whatever libraries it's looking for in the root file system.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    There are several reasons why this might happen, but I think the most likely cause is that the executable you are trying run is either compiled for the wrong word length, or there are dynamic libraries the executable requires that are not installed on the Ubuntu target.  You can check the file format by going to the directory on your target that contains your executable, and type:   file <executable name>.   You should get something back that indicates it is a 32-bit LSB executable for ARM if it is the correct format, in which case it likely will also tell you that it is dynamically linked.   If the latter is the case, then of course the solution is to install whatever libraries it's looking for in the root file system.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Ron,
    You're right, caused by missing .so libraries.
    it now works fine.
    Thank you!