Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Initialize and Access of 256KB OCM (SRAM)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 352 views
  • Users 0 members are here
Related

Initialize and Access of 256KB OCM (SRAM)

e14 Contributor
e14 Contributor over 13 years ago


During the boot time, the boot ROM will load the FSBL image from Flash to 192KB OCM (lower addr space).

I am wondering at what stage the unused 192KB and the upper 64KB OCM will be initialized? Is the initialization at BootROM or FSBL stage?

Is that a way that I can access the OCM before the initializaiton step or control the initialization process?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    No, You may not do anything with OCM until after the FSBL has finished loading (everything) and passes control back to the processors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks for the comments. When the BootROM loads the FSBL to OCM, will it first initialize the 192KB+64KB OCM to all zeros? I would like to check the power-up states of OCM SRAM but now I see all unused OCM intialized to zeros after FSBL. I am wondering whether I could customize the FSBL to extract the uninitialized OCM. However, if the 256KB OCM initiliazation is done at BootROM stage, then nothing could help. Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks for the comments. When the BootROM loads the FSBL to OCM, will it first initialize the 192KB+64KB OCM to all zeros? I would like to check the power-up states of OCM SRAM but now I see all unused OCM intialized to zeros after FSBL. I am wondering whether I could customize the FSBL to extract the uninitialized OCM. However, if the 256KB OCM initiliazation is done at BootROM stage, then nothing could help. Thanks.