Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development AXIDMA & FFT: no output
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 375 views
  • Users 0 members are here
Related

AXIDMA & FFT: no output

suppamax
suppamax over 10 years ago

Hi,



the zynq project I am working on is composed of PS, AXI-DMA and an FFT - it is a simplified version of this http://www.wiki.xilinx.com/Zynq-7000+AP+SoC+Spectrum+Analyzer+part+5+-+Accelerating+Software+-+Accelerating+an+FFT+with+ACP+Coprocessor+Tech+Tip.

As the original, I use an userspace IO driver.

The run_fft function terminates, so I assume the PS receives the interrupt indicating the end of the FFT calculation, but I see that the output buffer is untouched (I initialize it with 0xFF...FF before starting the FFT).

For debugging I modified the HW in PL, using a loopback instead of the FFT: in this case the output buffer contains a copy of the input.

How could I debug the FFT?
Why do I receive an interrupt from DMA (*) if no data has been written in the destination buffer?

(*) I use this command to wait for an irq
status = read(fd_uio, (void *) &pending, sizeof(int));
I also used
while (XAxiDma_Busy(&XAxiDmaInstance, XAXIDMA_DMA_TO_DEVICE)) ;
while (XAxiDma_Busy(&XAxiDmaInstance, XAXIDMA_DEVICE_TO_DMA)) ;
but result was the same


Thanks,
Max

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Max,

     

    You don't mention what version of the Xilinx tools you are using, but I find it useful to implement Xilinx Tech Tips initially in the Vivado Version they are targeted for to get a 'baseline' working system before making any modifications. This tech tip looks to be targeted to Vivado 2013.4.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Max,

     

    You don't mention what version of the Xilinx tools you are using, but I find it useful to implement Xilinx Tech Tips initially in the Vivado Version they are targeted for to get a 'baseline' working system before making any modifications. This tech tip looks to be targeted to Vivado 2013.4.

     

    -Gary