Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development DRAM to DDR issue in Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 363 subscribers
  • Views 1059 views
  • Users 0 members are here
Related

DRAM to DDR issue in Zedboard

e14 Contributor
e14 Contributor over 10 years ago

Hi.
I am facing issue with reading from DDR memory to PL(led's).
i have connected fabric hardware like shown in image on this link https://drive.google.com/folderview?id=0Byl0l4ua8ptEaXJ2SUFibVZJekk&usp=sharing , address allocated to all hardware are also shown in image.
also i have written following code for configuring hardware

----------------------------------------------------------------------------------------------------------------------------------------------------

CODE :
/*
* Copyright (c) 2009-2012 Xilinx, Inc.  All rights reserved.
*
* Xilinx, Inc.
* XILINX IS PROVIDING THIS DESIGN, CODE, OR INFORMATION "AS IS" AS A
* COURTESY TO YOU.  BY PROVIDING THIS DESIGN, CODE, OR INFORMATION AS
* ONE POSSIBLE   IMPLEMENTATION OF THIS FEATURE, APPLICATION OR
* STANDARD, XILINX IS MAKING NO REPRESENTATION THAT THIS IMPLEMENTATION
* IS FREE FROM ANY CLAIMS OF INFRINGEMENT, AND YOU ARE RESPONSIBLE
* FOR OBTAINING ANY RIGHTS YOU MAY REQUIRE FOR YOUR IMPLEMENTATION.
* XILINX EXPRESSLY DISCLAIMS ANY WARRANTY WHATSOEVER WITH RESPECT TO
* THE ADEQUACY OF THE IMPLEMENTATION, INCLUDING BUT NOT LIMITED TO
* ANY WARRANTIES OR REPRESENTATIONS THAT THIS IMPLEMENTATION IS FREE
* FROM CLAIMS OF INFRINGEMENT, IMPLIED WARRANTIES OF MERCHANTABILITY
* AND FITNESS FOR A PARTICULAR PURPOSE.
*
*/

/*
* helloworld.c: simple test application
*
* This application configures UART 16550 to baud rate 9600.
* PS7 UART (Zynq) is not initialized by this application, since
* bootrom/bsp configures it to baud rate 115200
*
* ------------------------------------------------
* | UART TYPE   BAUD RATE                        |
* ------------------------------------------------
*   uartns550   9600
*   uartlite    Configurable only in HW design
*   ps7_uart    115200 (configured by bootrom/bsp)
*/

#include <stdio.h>
#include "platform.h"
#include "ps7_init.h"
#include <xil_io.h>
#include "xscugic.h"
#include "xparameters.h"

/********************************Write Data**********************************/
void StartDMATransfer (unsigned int dest_addr , unsigned int length)
{
tu32 addr1;
tu32 addr2;

taddr1 = XPAR_AXI_DMA_0_BASEADDR + 0x48;
taddr2 = XPAR_AXI_DMA_0_BASEADDR + 0x58;
t//Writing Address to S2MM_DA register
tXil_Out32(addr1 , dest_addr);
t//Writing Length to S2MM_LENGTH register
tXil_Out32(addr2 , length);
}
/********************************Read Data**********************************/
void Read_Data (unsigned int dest_addr , unsigned int length)
{
ttu32 addr1;
ttu32 addr2;

ttaddr1 = XPAR_AXI_DMA_1_BASEADDR + 0x18;
ttaddr2 = XPAR_AXI_DMA_1_BASEADDR + 0x28;
tt//Writing Address to MM2S_DA register
ttXil_Out32(addr1 , dest_addr);
tt//Writing Length to MM2S_LENGTH register
ttXil_Out32(addr2 , length);
}

/*******************Interrupt_Handler*******************/
XScuGic InterruptController0;
XScuGic InterruptController1;
static XScuGic_Config *GicConfig0;
static XScuGic_Config *GicConfig1;
u32 frame_count0;
u32 frame_count1;

/*************************Write Interrupt***********************/
void InterruptHandler1(void)
{
tu32 tmpval;
tu32 addr1;

taddr1 = XPAR_AXI_DMA_0_BASEADDR + 0x34;
t// xil_printf("Interrupt Acknowledgment.
r");

t// Interrupt clear and write to bit no. 12 of S2MM_DMASR
ttmpval = Xil_In32(addr1);
ttmpval = tmpval | 0x1000;
tXil_Out32(addr1,tmpval);

t//DRAM DATA PROCESSING
tframe_count1++;
tif(frame_count1 > 10000000)
t{
ttxil_printf("Frame Number write : %d
r",frame_count1);
ttreturn ;
t}

t//initiate DATA Transfer
t//StartDMATransfer(0xa000000+128*frame_count,256);
tStartDMATransfer( 0xa000000, 256);
}

int SetupInterruptSys1(XScuGic *XScuGicInstancePtr1)
{
tXil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_INT,(Xil_ExceptionHandler) XScuGic_InterruptHandler,XScuGicInstancePtr1);
tXil_ExceptionEnable();
treturn XST_SUCCESS;
}

int Initial_Interrupt1(deviceID1)
{
tint status;

tGicConfig1 = XScuGic_LookupConfig (deviceID1);
tif(NULL == GicConfig1 )
t{
ttreturn XST_FAILURE;
t}

tstatus = XScuGic_CfgInitialize (&InterruptController1,GicConfig1,GicConfig1->CpuBaseAddress);
tif(status != XST_SUCCESS)
t{
ttreturn XST_FAILURE;
t}

tstatus = SetupInterruptSys1( &InterruptController1 );
tif(status != XST_SUCCESS)
tt{
tttreturn XST_FAILURE;
tt}

tstatus = XScuGic_Connect (&InterruptController1,
tttXPAR_FABRIC_AXI_DMA_0_S2MM_INTROUT_INTR,
ttt(Xil_ExceptionHandler)InterruptHandler1,
tttNULL);
tif(status != XST_SUCCESS)
ttt{
ttttreturn XST_FAILURE;
ttt}

tXScuGic_Enable (&InterruptController1 , XPAR_FABRIC_AXI_DMA_0_S2MM_INTROUT_INTR);

treturn XST_SUCCESS;
}

/*************************Read Interrupt************************/
void InterruptHandler0(void)
{
tu32 tmpval;
tu32 addr1;

ttaddr1 = XPAR_AXI_DMA_1_BASEADDR + 0x04;
t// xil_printf("Interrupt Acknowledgment.
r");

t// Interrupt clear and write to bit no. 12 of S2MM_DMASR
ttmpval = Xil_In32(addr1);
ttmpval = tmpval | 0x1000;
tXil_Out32(addr1,tmpval);

t//DRAM DATA PROCESSING
tframe_count0++;
tif(frame_count0 > 10000000)
t{
ttxil_printf("Frame Number Read: %d
r",frame_count0);
ttreturn ;
t}

t//initiate DATA Transfer
t//StartDMATransfer(0xa000000+128*frame_count,256);
tRead_Data(0xa00000c, 256);
}
int SetupInterruptSys0(XScuGic *XScuGicInstancePtr0)
{
tXil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_INT,(Xil_ExceptionHandler) XScuGic_InterruptHandler,XScuGicInstancePtr0);
tXil_ExceptionEnable();
treturn XST_SUCCESS;
}

int Initial_Interrupt0(deviceID0)
{
tint status;

tGicConfig0 = XScuGic_LookupConfig (deviceID0);
tif(NULL == GicConfig0 )
t{
ttreturn XST_FAILURE;
t}

tstatus = XScuGic_CfgInitialize (&InterruptController0,GicConfig0,GicConfig0->CpuBaseAddress);
tif(status != XST_SUCCESS)
t{
ttreturn XST_FAILURE;
t}

tstatus = SetupInterruptSys0( &InterruptController0 );
tif(status != XST_SUCCESS)
tt{
tttreturn XST_FAILURE;
tt}

tstatus = XScuGic_Connect (&InterruptController0,
tttXPAR_FABRIC_AXI_DMA_1_MM2S_INTROUT_INTR,
ttt(Xil_ExceptionHandler)InterruptHandler0,
tttNULL);
tif(status != XST_SUCCESS)
ttt{
ttttreturn XST_FAILURE;
ttt}

tXScuGic_Enable (&InterruptController0 , XPAR_FABRIC_AXI_DMA_1_MM2S_INTROUT_INTR);

treturn XST_SUCCESS;
}

/********************************Initialize DMA**********************************/
int Initial_AXI_DMA(void)
  {
ttunsigned int tmp0;
ttunsigned int tmp1;

ttu32 addr1;
ttu32 addr2;

ttaddr2 = XPAR_AXI_DMA_1_BASEADDR + 0x00;
ttaddr1 = XPAR_AXI_DMA_0_BASEADDR + 0x30;
tt// setting S2MM DMACR.RS = 1
tttmp0 = Xil_In32(addr1); // read from address 0x40400000 + 0x30
tttmp0 = tmp0 | 0x1001; // Modifying value // enable data unit & interrupt when done
ttXil_Out32(addr1,tmp0); // writing back to the same address 0x40400000 + 0x30
tttmp0 = Xil_In32(addr1);
ttxil_printf("DMA S2MM Control Register Value is %x
r",tmp0);

tt// setting MM2S DMACR.RS = 1
tttmp1 = Xil_In32(addr2); // read from address 0x40400000 + 0x30
tttmp1 = tmp1 | 0x1001; // Modifying value // enable data unit & interrupt when done
ttXil_Out32(addr2,tmp1); // writing back to the same address 0x40400000 + 0x30
tttmp1 = Xil_In32(addr2);
ttxil_printf("DMA MM2S Control Register Value is %x
r",tmp1);

ttreturn 0;
  }
/*******************My_ip*******************************/
int Initial_My_IP(unsigned int size)
{
tXil_Out32(XPAR_AXI_GPIO_0_BASEADDR, size); // set Frame Size
tXil_Out32(XPAR_AXI_GPIO_1_BASEADDR, 1); // Enable to generate Samples

treturn 0;
}
/*****************************MAIN***************************/
int main()
{
    init_platform();

    ps7_post_config();

    char c;

    unsigned int d;

    xil_printf("Initializing AXI_DMA
r"); // Initializing DMA
    Initial_AXI_DMA();

    xil_printf("Do You Want To Perform Write.....?
r");
    xil_printf("y for Yes or n for No
r");
    c= getchar();

    if(c=='w')
    {
    txil_printf("Enabling My_ip to Generate Samples ............
r"); // Initializing My_IP
    tInitial_My_IP(64); // End of frame after 128 Bytes (32 words) transferred

    txil_printf("Enabling Write Interrupt Handler ...........
r"); // Initializing Interrupts
    tInitial_Interrupt1(XPAR_PS7_SCUGIC_0_DEVICE_ID);

    txil_printf("Writing Begins...........
r"); // Initial DMA Transfer
    tStartDMATransfer( 0xa000000, 256);
    tc = 'a';
    }
    else if(c=='r')
    {
    tXil_DCacheDisable();

    txil_printf("Enabling read Interrupt Handler ...........
r"); // Initializing Interrupts
    tInitial_Interrupt0(XPAR_PS7_SCUGIC_0_DEVICE_ID);

    txil_printf("Reading Begins...........
r"); // Initial DMA Transfer
    tRead_Data(0xa000004,256);
    tc = 'a';
    td = Xil_In32(0xa000004);
    txil_printf("value = %d
r",d);
    }
    else
    {
    tc='a';
    }
    return 0;
}
----------------------------------------------------------------------------------------------------------------------------------------------------
ISSUES :
1- Reading abrupt values but able to see the correct value.
2- Writing correct values but don't it is uncontrollable.
3- Need a proper explanation.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

     

    It looks like you have a lot going on at once and you did not give us much information. You should always note what version of the Xilinx tools you are using, your host PC OS, what you are trying to accomplish. and a detailed description of the problem. It is not clear to me exactly what problem you are seeing.

     

    I doubt anyone will have the time to pore over your whole hardware diagram and your lengthy code snippet, but I do have a couple of suggestions.

     

    In your code there is mention of a UART in addition to the ps uart due to needing 9600 baud, but I don't see another UART in your hardware. If you just want to change the baud rate of the ps uart you can take a look at this forum post:

     

    http://zedboard.org/content/configure-uart-baud-rate

     

    As to the memory interface I would suggest testing your hardware by making direct memory reads and writes before attempting DMA transfers. Then, if that works, start adding DMAs. You might want to look at the example code for the axi dma available in the SDK system.mss.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

     

    It looks like you have a lot going on at once and you did not give us much information. You should always note what version of the Xilinx tools you are using, your host PC OS, what you are trying to accomplish. and a detailed description of the problem. It is not clear to me exactly what problem you are seeing.

     

    I doubt anyone will have the time to pore over your whole hardware diagram and your lengthy code snippet, but I do have a couple of suggestions.

     

    In your code there is mention of a UART in addition to the ps uart due to needing 9600 baud, but I don't see another UART in your hardware. If you just want to change the baud rate of the ps uart you can take a look at this forum post:

     

    http://zedboard.org/content/configure-uart-baud-rate

     

    As to the memory interface I would suggest testing your hardware by making direct memory reads and writes before attempting DMA transfers. Then, if that works, start adding DMAs. You might want to look at the example code for the axi dma available in the SDK system.mss.

     

    -Gary