Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Programming vpga via  Linux. Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 310 views
  • Users 0 members are here
Related

Programming vpga via  Linux. Zedboard

e14 Contributor
e14 Contributor over 11 years ago

Hello everyone!

I'm in a middle of a project, I will describe it to you:
In vivdo I have used the board of Zedboard, and I used the ip core of the Zynq 7000.
I have also add an axi fifo (but it could be any other peripheral) I have connected the fifo to the Zynq processor ip core.

Now I know I can export my design and "to program" the fifo via the sdk of vivdo.
But I want to program it on the operating system I have on the zedboard - Linux.
For example, in the c code I wirte data to the fifo..
How do I do it?

I have already read this guide:

http://www.fpgadeveloper.com/2014/08/creating-a-custom-ip-block-in-vivado.html

But here he just check his ipcore with the sdk. I want to program(to talk ) with the peripherals via the code on the Linux. (Sorry about my English i hope you understand what do I need..)

So if you have a guide or you can explain me it will be wonderful!
Thank you!
Idan.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    You might want to download the Avnet  PetaLinux for the ZynqRegistered-7000 All Programmable SoC  Speedway workshop on PetaLinux.

     

    There is also thread on the Xilinx Embedded Linux community forum that should be helpful. It is a little involved, especially if you follow the links (and their links), but it should give you a good place to start on the subject.

     

    http://forums.xilinx.com/t5/Embedded-Linux/Petalinux-loadable-Kernel-Module-Tutorial/td-p/546927

     

    -Gary