Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development OpenCV on ZedBoard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 364 subscribers
  • Views 1594 views
  • Users 0 members are here
Related

OpenCV on ZedBoard

e14 Contributor
e14 Contributor over 14 years ago

Has anyone been able to successfully install OpenCV on the ZedBoard?  I get an internal compiler error, which I believe has to do with the lack of a GPU.  I've glanced briefly at the make file to try to figure out a way around this but so far no luck.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    If you don't want it to run as a standalone then try this.  Firstly you need to cross compile the libraries using the arm-xilinx-linux-gcc which Xilinx provide.  I would suggest compiling them as static unless you want to generate a new ramdisk image with enough space for the shared libraries.  After that in SDK you can create a C Linux application but change the compiler and linker to g++ (rather than gcc) and add "-static -lstdc++" to the linker flags (again unless you want to change the ramdisk to include C++ libs).  It will throw up a lot of unused function warnings, but you can turn those off and it works fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    If you don't want it to run as a standalone then try this.  Firstly you need to cross compile the libraries using the arm-xilinx-linux-gcc which Xilinx provide.  I would suggest compiling them as static unless you want to generate a new ramdisk image with enough space for the shared libraries.  After that in SDK you can create a C Linux application but change the compiler and linker to g++ (rather than gcc) and add "-static -lstdc++" to the linker flags (again unless you want to change the ramdisk to include C++ libs).  It will throw up a lot of unused function warnings, but you can turn those off and it works fine.