Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development OpenCV on ZedBoard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 364 subscribers
  • Views 1592 views
  • Users 0 members are here
Related

OpenCV on ZedBoard

e14 Contributor
e14 Contributor over 14 years ago

Has anyone been able to successfully install OpenCV on the ZedBoard?  I get an internal compiler error, which I believe has to do with the lack of a GPU.  I've glanced briefly at the make file to try to figure out a way around this but so far no luck.

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 14 years ago

    I've heard of a few looking at this, but I have not heard of any successes yet.  The Zynq PS does not have a built-in GPU, so you will have to build that in the programmable logic.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to bhfletcher

    I've been able to get OpenCV to work, although it's somewhat hindered.  Anything with GPU acceleration is obviously not going to work, and because of the ARM processor you don't get the convenient automatic threading you get with Intel processors.  Besides that some dependencies don't work with ARM, and as far as I can tell some that should work with ARM just won't work on this board. 

    I built it within Xillinux rather than try to cross-compile it.  Obviously cross-compiling has its advantages but there are so many dependencies I haven't even tried yet.

    If you follow this guide (http://www.samontab.com/web/2012/06/installing-opencv-2-4-1-ubuntu-12-04-lts/), ignoring the steps about apt-get update and apt-get upgrade (if you do this you will not be able to reboot or recover and have to reformat your SD card), removing any dependencies it says it can't find (there are a lot), ignoring the warnings, it will install and you have a partially working OpenCV library.  As of yet, I can't really figure out why some parts work and some parts don't, but it's a starting point.

    I'm doing this on the compressed xillinux 3.3 kernel, not the full Digilent kernel.  The Digilent kernel has given me nothing but trouble.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I am trying to install opencv on Xillinux as described in the link, after installing cmake when i reach to this commnad

    root@localhost:~/OpenCV-2.4.1/build# cmake -DWITH_TBB=ON -DWITH_V4L=ON -DINSTALL_C_EXAMPLES=ON -DBUILD_EXAMPLES=ON
    iget this error
    CMake Error: The source directory "/root/OpenCV-2.4.1/build" does not appear to contain CMakeLists.txt.
    Specify --help for usage, or press the help button on the CMake GUI.

    can u help me with this. or may be share with me what exactly you did to get opencv running on zedboard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I am trying to install opencv on Xillinux as described in the link, after installing cmake when i reach to this commnad

    root@localhost:~/OpenCV-2.4.1/build# cmake -DWITH_TBB=ON -DWITH_V4L=ON -DINSTALL_C_EXAMPLES=ON -DBUILD_EXAMPLES=ON
    iget this error
    CMake Error: The source directory "/root/OpenCV-2.4.1/build" does not appear to contain CMakeLists.txt.
    Specify --help for usage, or press the help button on the CMake GUI.

    can u help me with this. or may be share with me what exactly you did to get opencv running on zedboard