Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development AXI GPIO Interrupt
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 364 subscribers
  • Views 4853 views
  • Users 0 members are here
Related

AXI GPIO Interrupt

e14 Contributor
e14 Contributor over 11 years ago

Hello everyone,

i'd like to use an interrupt from a pushbutton. The buttons are connected via axi_gpio (IOCarrierCard). They works in uio in petalinux. I can read the value of the 4 pushbuttons in uio.
Now i try to detect an interrupt.
I enabled interrupts in axi_gpio ip and fabric interrupts and IRQ_F2P in zynq processing system. After that i connected them.
In the kernel config i activated "userspace i/o drivers", "userspace i/o platform driver with irq..." and "xilinx axi performance monitor driver".
My system-top.dts looks like:

&axi_gpio_0 {
ttcompatible = "generic-uio";
                interrupts = <0 29 4>;
ttinterrupt-parent = <&intc>;
t};

After booting the system and push the buttons, i don't see an interrupt with "cat /proc/interrupt" (i see  61:          0          0       GIC  61  gpio ).
I also try to write a user application and wait for an interrupt with:

int irq_count = 0;
... open and map uio ....
if(read(fd, &irq_count, 4) != 4)
t{
ttperror("read uio0");
               
t}
printf("Interrupt!");

I think after receiving an interrupt, the programm should print "Interrupt" but nothing happpens.

I followed this tutorial: http://svenand.blogdrive.com/archive/150.html#.VWRsV0YQjph


My setup:
Petalinux, SDK, Vivado 2014.4
Microzed Board with IOCarrier Card

Thanks for your answers,
Sebastian

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi Sebastian,

    Do you know which FPGA to Processor (F2P) interrupt you are using?

    If you know that you are only using one interrupt then it likely got assigned to F2P_INT0 which according to xparameters_ps.h in a Standalone BSP is defined as interrupt 61:

    #define XPS_FPGA0_INT_IDtt61

    So I think the interrupt math works out to what you have in the DTS okay 61 - 32 = 29 so I don't think the problem is in the DTS.

    Can you post more of your code which shows what device you are opening and how you are mmap-ing?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi Sebastian,

    Do you know which FPGA to Processor (F2P) interrupt you are using?

    If you know that you are only using one interrupt then it likely got assigned to F2P_INT0 which according to xparameters_ps.h in a Standalone BSP is defined as interrupt 61:

    #define XPS_FPGA0_INT_IDtt61

    So I think the interrupt math works out to what you have in the DTS okay 61 - 32 = 29 so I don't think the problem is in the DTS.

    Can you post more of your code which shows what device you are opening and how you are mmap-ing?

    Regards,

    -Kevin