Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development AXI GPIO Interrupt
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 364 subscribers
  • Views 4853 views
  • Users 0 members are here
Related

AXI GPIO Interrupt

e14 Contributor
e14 Contributor over 11 years ago

Hello everyone,

i'd like to use an interrupt from a pushbutton. The buttons are connected via axi_gpio (IOCarrierCard). They works in uio in petalinux. I can read the value of the 4 pushbuttons in uio.
Now i try to detect an interrupt.
I enabled interrupts in axi_gpio ip and fabric interrupts and IRQ_F2P in zynq processing system. After that i connected them.
In the kernel config i activated "userspace i/o drivers", "userspace i/o platform driver with irq..." and "xilinx axi performance monitor driver".
My system-top.dts looks like:

&axi_gpio_0 {
ttcompatible = "generic-uio";
                interrupts = <0 29 4>;
ttinterrupt-parent = <&intc>;
t};

After booting the system and push the buttons, i don't see an interrupt with "cat /proc/interrupt" (i see  61:          0          0       GIC  61  gpio ).
I also try to write a user application and wait for an interrupt with:

int irq_count = 0;
... open and map uio ....
if(read(fd, &irq_count, 4) != 4)
t{
ttperror("read uio0");
               
t}
printf("Interrupt!");

I think after receiving an interrupt, the programm should print "Interrupt" but nothing happpens.

I followed this tutorial: http://svenand.blogdrive.com/archive/150.html#.VWRsV0YQjph


My setup:
Petalinux, SDK, Vivado 2014.4
Microzed Board with IOCarrier Card

Thanks for your answers,
Sebastian

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Kevin,

    I solved the problem with printf(). If puts() is used, it works.

    I checked the buttons for bouncing with a oscilloscope. Thats not the problem. I print a counter for interrupts in the terminal. The same effect as "cat /proc/interrupt".
    I modified my DTS in

    interrupts = <0 29 1>; //rising edge
    1 interrupt for rising edge, 1 interrupt for falling edge
    "cat /pproc/..."=1 and my "counter"=1

    interrupts = <0 29 4>; // high level
    2 interrupts for rising edge, 2 interrupts for falling edge
    "cat /pproc/..."=4 and my "counter"=2

    regards,
    Sebastian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Kevin,

    I solved the problem with printf(). If puts() is used, it works.

    I checked the buttons for bouncing with a oscilloscope. Thats not the problem. I print a counter for interrupts in the terminal. The same effect as "cat /proc/interrupt".
    I modified my DTS in

    interrupts = <0 29 1>; //rising edge
    1 interrupt for rising edge, 1 interrupt for falling edge
    "cat /pproc/..."=1 and my "counter"=1

    interrupts = <0 29 4>; // high level
    2 interrupts for rising edge, 2 interrupts for falling edge
    "cat /pproc/..."=4 and my "counter"=2

    regards,
    Sebastian