Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Using /dev/mem to read/write SPI controller
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 362 subscribers
  • Views 717 views
  • Users 0 members are here
Related

Using /dev/mem to read/write SPI controller

miantang
miantang over 8 years ago

Hi, I'm using MicroZed board, and try to read/write SPI registers via /dev/mem. However, each time when I use devmem2 to write data to SPI registers, the value read back is always zero, like below:

root@xxxxxx:~# devmem2 0xe0006000 w 0x27e19

    /dev/mem opened. Memory mapped at address 0xb6fda000.

    Value at address 0xE0006000 (0xb6fda000): 0x0 Written 0x27E19; readback 0x27E19

root@xxxxxx:~# devmem2 0xe0006000

    /dev/mem opened. Memory mapped at address 0xb6eff000.

    Value at address 0xE0006000 (0xb6eff000): 0x0

 

And Here is what I did in my design:

a) I use Vivado to create hardware design based on MicroZed board, and only add SPI0 and SPI1. It seems EMIO is used for SPI0 and MIO for SPI1. After that, I just sync, implementation, and generate bitstream and HDF file.

 

b) I import HDF into Petalinux, and enable the following SPI configuration in kernel:

    Cadence SPI Controller

    Xilinx SPI controller common module

    Xilinx Zynq QSPI controller

    User mode SPI device driver support

 

c) Then, run petalinux-build.

 

d) I copy BOOT.BIN and image.ub to MicroZed board, and run. At this time, I use devmem2 to read/write both SPI0 and SPI1, the physical address is 0xe0006000 and 0xe0007000.

 

Am I missing something during steps above? Please give me some hints or suggestions. Thank a lot.