Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development QSPI flash memory programming issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 562 views
  • Users 0 members are here
Related

QSPI flash memory programming issue

zsv
zsv over 8 years ago

There is board with SoC Zynq-7000, i'm working with qspi flash memory S25FL256S. There is no problem when i program memory with bytecount 4, 8, 12 - amount multiple of 4. 

 

What have i do to program memory with 1, 2 or 3 byte? 

  • Sign in to reply
  • Cancel
  • zsv
    0 zsv over 8 years ago

    The problem was solved. You can not write 1,2,3 bytes in automatic CS management mode. You need to set manual CS, and make next sequence. For example, we use command PP=0x02 with 3 bytes address, and we want to write 1 byte 0xAB at address = 0x01

     

    1. Set flash WriteEnable, after execution of WE-command CS must be at 1

    2. Set CS to 0

    3. XQspiPs_WriteReg(QSPI_BASEADDR, XQSPIPS_TXD_01_OFFSET, 0x02);

    4. Execute ManualStart();

    5. Wait for TX FIFO empty

    6. XQspiPs_WriteReg(QSPI_BASEADDR, XQSPIPS_TXD_00_OFFSET, 0xAA010000);

    7. Execute ManualStart();

    8. Wait for TX FIFO empty

    9. Set CS to 1

    10. Life is good

     

    Thank's everybody for help :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer