Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development MicroZed: Unable to boot from SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 636 views
  • Users 0 members are here
Related

MicroZed: Unable to boot from SD card

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I am trying to get my MicroZed running. Booting from the pre-programmed QSPI-Flash works without any problems. The default SD card image that can be downloaded from the MicroZed website throws an error while u-boot tries to write the bitstream to the PL, but I can get it to boot. However, if I generate my own BOOT.bin file in the SDK, nothing happens. I created a FSBL project based upon the hardware files I exported from Vivado (2014.2). I ensured that the FSBL is the first partition and marked as bootloader, I put my .bit file as the second partition and u-boot.elf as the third. Both as datafile. I also tried omitting my .bit file or including files like uImage and uramdisk.image.gz. Nothing works. My serial terminal is configured right, as I am able to see the output if I boot from QSPI. I added the FSBL_DEBUG_INFO as suggested in AR# 59476, but that didn't gave me any output either. Even if I take the FSBL and u-boot.elf from the MicroZed tutorial 04, I can't get a bootable BOOT.bin. What might I be doing wrong?

Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Have you tried a different micro SD Card to rule out a problem with the card itself?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    It's exactly the same with an other SD card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Has no one an idea? It would also be very helpful if someone could build a BOOT.bin with the SDK for me, just using a fsbl and u-boot. If you could then provide me with the BOOT.bin, the fsbl.elf and the u-boot.elf, I could check if the problem is my SDK or my MicroZed.

    Oh and I have the 7020 version.

    Thanks