Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Download petalinux image to zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 869 views
  • Users 0 members are here
Related

Download petalinux image to zedboard

cascade99
cascade99 over 10 years ago

Hi,
I used petalinux-build to create the following images, I suppose using "petalinux-package --boot --fsbl <FSBL image> --fpga <FPGA bitstream> --uboot" to create .bin file, my question is where should I find FPGA bitstream file? I used Avnet-Digilent-ZedBoard-2014.4.bsp as hardware description when I built.

Here is my files I have:

-rwxr-xr-x. 1 root root 10364648 Jan 28 14:32 image.elf
-rw-r--r--. 1 root root  6882792 Jan 28 14:33 image.ub
-rw-r--r--. 1 root root  7820288 Jan 28 14:32 rootfs.cpio
-rw-r--r--. 1 root root  3485304 Jan 28 14:32 rootfs.cpio.gz
-rw-r--r--. 1 root root    14403 Jan 28 15:20 system.dtb
-rw-r--r--. 1 root root  1837275 Jan 28 15:20 System.map.linux
-rwxr-xr-x. 1 root root   274308 Jan 28 15:21 u-boot.bin
-rwxr-xr-x. 1 root root  1577796 Jan 28 15:21 u-boot.elf
-rwxr-xr-x. 1 root root   274308 Jan 28 14:33 u-boot-s.bin
-rwxr-xr-x. 1 root root  1577796 Jan 28 14:33 u-boot-s.elf
-rwxr-xr-x. 1 root root   823018 Jan 28 15:21 u-boot.srec
-rwxr-xr-x. 1 root root   823056 Jan 28 14:33 u-boot-s.srec
-rw-r--r--. 1 root root  3485368 Jan 28 14:32 urootfs.cpio.gz
-rwxr-xr-x. 1 root root 13614759 Jan 28 15:20 vmlinux
-rwxr-xr-x. 1 root root  6883568 Jan 28 14:33 zImage
-rwxr-xr-x. 1 root root   245115 Jan 28 13:35 zynq_fsbl.elf


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The BSP contains the btstream in <petalinux-project>/pre-built//linux/implementation/download.bit.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The BSP contains the btstream in <petalinux-project>/pre-built//linux/implementation/download.bit.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • cascade99
    0 cascade99 over 10 years ago in reply to e14 Contributor

    Thank you. That's it.