Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Using Zed Touch Display Kit (7 or 10) with PetaLinux?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 640 views
  • Users 0 members are here
Related

Using Zed Touch Display Kit (7 or 10) with PetaLinux?

armendzh
armendzh over 10 years ago

I have Mini-ITX board and want to use it together with Zed Touch Display Kit (10 inch version) using PetaLinux.

What do I need to do to make it work?

When using hdf file from the Zed Touch Display Kit reference design for Mini-ITX board to build my PetaLinux project (from AVNET github), I am getting this error when I try to boot the compiled Linux image:
https://github.com/Avnet/hdl
======
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
dma-pl330 f8003000.dmac:        DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
======
I am guessing I don't have module or driver in the kernel to make it recognize the display.

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi armendzh,

    We offer a standalone 2015.2 reference design for each of these display panels which will demonstrate the capabilities of the hardware.

    We are looking to add support for the display kits to Wind River Pulsar Linux to give us a path for ongoing support.

    However, we currently do not have support for either of the display kits under PetaLinux and this would require some patching to the Linux kernel that comes with PetaLinux to setup the VDMA properly.

    Are you working with a local Avnet/Silica FAE on your design?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • armendzh
    0 armendzh over 10 years ago in reply to zedhed

    Hi Kevin.

    Yes, I have used those reference designs to get hdf file to build my PetaLinux project.
    When do you expect support for Wind River Pulsar linux to be available? I am still not sure how I can use PL designs with Wind River Pulsar Linux, reason why I was going embedded with PetaLinux.

    Is you my only option now is to try to apply same patch found in the MicroZed_ALI3_Display_Ubuntu_Tutorial_14_4_02 design reference for 7" display kit? Would it work for 10" display kit?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • armendzh
    0 armendzh over 10 years ago in reply to armendzh

    Do I apply patch inside PetaLinux directory?
    $PETALINUX/components/linux-kernel/xlnx-3.19

    or at the PetaLinux project files?