Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Invalidating the data cache
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 364 subscribers
  • Views 4770 views
  • Users 0 members are here
Related

Invalidating the data cache

e14 Contributor
e14 Contributor over 11 years ago

I have a problem that I am trying to fix in a program I have written.

I receive internet packets, the Rx interrupt affects a bool so that in a loop I can to to then request the RxBD from the hardware. I then copy out the packets into some linked list containers that I have before returning the BDs to the hardware.


My problem is that when I go to read the data that the BD points to, the cached data is wrong, so I invalidate it. Except that using

void Xil_DCacheInvalidateRange(unsigned int adr, unsigned len)

invalidates a cache line but not necessarily where the packet information starts. It looks at the address I pass to it, then it moves from there to the start of the first cache line and only then begins invalidating the cache.


This leads to varying parts of my packet information being "chopped off". Anywhere from 0 to 28 bytes worth of data.


A solution to this, as stated in the Xilinxs documentation seems to be to cache align the... sections of memory that the BD point to. The problem is, I have no idea how to do this.


I have tried simply disabling the entire cache at the start of the program, however this doesn't seem to work. I don't know if it is my attempt that doesn't work, or if it simply doesn't fix the problem.

(Code used to try to disable the entire cache)
Xil_L2CacheDisable();
Xil_L1DCacheDisable();
Xil_L1ICacheDisable();
dsb();
isb();

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Where do you get this error? In which function? Try to singlestep with the debugger.

    You cannot simply use Xil_SetTlbAttributes(RX_BD_START_ADDRESS, 0xc02); because here RX_BD_START_ADDRESS must be a multiple of 1MB.

    If you do Xil_DCacheDisable() in the verry beginning of your program, you will not have cacheing problems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Where do you get this error? In which function? Try to singlestep with the debugger.

    You cannot simply use Xil_SetTlbAttributes(RX_BD_START_ADDRESS, 0xc02); because here RX_BD_START_ADDRESS must be a multiple of 1MB.

    If you do Xil_DCacheDisable() in the verry beginning of your program, you will not have cacheing problems.