Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development How to run two different task parallely on two standalone processors on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 364 subscribers
  • Views 926 views
  • Users 0 members are here
Related

How to run two different task parallely on two standalone processors on Zedboard

e14 Contributor
e14 Contributor over 13 years ago

I am new to Zed board.I want to run two different task on two different standalone processors without load any OS on those processors.Like one processor will do sum of two integers and other processor will do multiply two nos. at a same time in Simple C program.suggest me some solution.Thank you.

  • Sign in to reply
  • Cancel
  • ejubenville
    0 ejubenville over 13 years ago

    Take a look at appnote 1079.  It address bare-metal applications running independently on both Cortex A9 processors on the ZC702 development board.  I seem to recall seeing instructions to adapt that example for a ZedBoard.

    http://www.xilinx.com/support/documentation/application_notes/xapp1079-amp-bare-metal-cortex-a9.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Also check out the latest information wiki.
    http://www.wiki.xilinx.com/XAPP1079+Latest+Information

    What you want to do is actually very simple. Alot more simple than involving Linux.

    XAPP 1079 involves writing 2 programs though, and putting them on separate cores. Not sure if that's how you want it...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Thank you.Please help me in the another scenario like sum of two nos. done in first processor and then result should go to another processor and multiplication it with another integer on second processor.
    Example:
    First Processor:result=a + b;
    Second Processor: result1=result*c;
    Can you please how to manage inter processor communication?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Default OCM (On Chip Memory) locations are 0x00000000 to 0x0002FFFF (low 64kB) as well as 0xFFFF0000 to 0xFFFFFFFF (high 64kB). You can see this in the default linker script (lscript.ld) under ram_0 and ram_1. OCM is common to both processors. So you could store your result in OCM and then both processors could access it. You'll need to explicitly identify what address you want to store your variable at. So do something like this (in both CPU0's and CPU1's source code):

    volatile u32 *result = (volatile u32 *)(0xFFFF0000);
    CPU0: *result = a + b;
    // set flag telling cpu1 that first operation has completed
    CPU1: result1 = *result * c;

    or do something simpler with a #define
    #define RESULT *(volatile u32 *)(0xFFFF0000)
    CPU0: RESULT = a + b;
    // set flag telling cpu1 that first operation has completed
    CPU1: result1 = RESULT * c;

    In both cases, you'll have to have a flag to communicate between the two processors (which will also need to be common to both cores, in OCM), telling each processor when the other has completed its task. If you try and operate on the same memory location with both CPUs at the same time, results will be unpredictable and probably undesirable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thank you.This will be helpful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I implemented and run xapp1079 but when I am trying to run it from flash memory,it is not load cpu1 application.Is it possible to run xapp 1079 from flash?
    A application on cpu0 is running from flash but from cpu1 it can't.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    CPU 0 willboot up first,then it will awak cpu 1 by SEV