Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Severe Network Issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 435 views
  • Users 0 members are here
Related

Severe Network Issue

e14 Contributor
e14 Contributor over 13 years ago

I recently created a test program that simply receives data as fast as possible and sends some data also via TCP using the Zedboard ethernet port running at a giga-bit.

Occasional I get the following error on the console.   The only way to get networking to work again is to reboot?   Anyone else seen this?  Any solution?

The only other thing to note is CPU#0 was 100% utilized mostly with system and interrupt time to handle this.

Kernel: 3.6.0-xilinx #1 SMP PREEMPT

WARNING: at net/sched/sch_generic.c:255 dev_watchdog+0x15c/0x26c()                                                                      
NETDEV WATCHDOG: eth0 (xemacps): transmit queue 0 timed out                                                                                                                                    
[<c0013fdc>] (unwind_backtrace+0x0/0x11c) from [<c0020e6c>] (warn_slowpath_common+0x4c/0x64)                                                   
[<c0020e6c>] (warn_slowpath_common+0x4c/0x64) from [<c0020f04>] (warn_slowpath_fmt+0x2c/0x3c)                                                     
[<c0020f04>] (warn_slowpath_fmt+0x2c/0x3c) from [<c0300de0>] (dev_watchdog+0x15c/0x26c)                                                           
[<c0300de0>] (dev_watchdog+0x15c/0x26c) from [<c002cbc0>] (run_timer_softirq+0x190/0x244)                                                         
[<c002cbc0>] (run_timer_softirq+0x190/0x244) from [<c0027350>] (__do_softirq+0xb8/0x174)                                                           
[<c0027350>] (__do_softirq+0xb8/0x174) from [<c0027860>] (irq_exit+0x48/0xa0)                                                                     
[<c0027860>] (irq_exit+0x48/0xa0) from [<c000e920>] (handle_IRQ+0x7c/0xb8)                                                                        
[<c000e920>] (handle_IRQ+0x7c/0xb8) from [<c0008484>] (gic_handle_irq+0x38/0x5c)                                                                   
[<c0008484>] (gic_handle_irq+0x38/0x5c) from [<c000dc80>] (__irq_svc+0x40/0x70)                                                                   
Exception stack(0xde06bfa0 to 0xde06bfe8)                                                                                                         
bfa0: de06a030 c000ebac de06bff0 00000000 1e05c06a 00000015 10c0387d c0554bf4                                                                     
bfc0: 0000406a 413fc090 00000000 00000000 00000000 de06bfe8 c000ebcc c000ebd0                                                                     
bfe0: 60000013 ffffffff                                                             
[<c000dc80>] (__irq_svc+0x40/0x70) from [<c000ebd0>] (default_idle+0x24/0x2c)                                                                     
[<c000ebd0>] (default_idle+0x24/0x2c) from [<c000edd0>] (cpu_idle+0xa0/0xfc)                                         
[<c000edd0>] (cpu_idle+0xa0/0xfc) from [<00383594>] (0x383594)                                                   
---[ end trace 97652d78abb4988e]---                                                 
xemacps e000b000.ps7-ethernet: transmit timeout 3000 ms, reseting...                                                  
BUG: scheduling while atomic: swapper/1/0/0x00000105                                                                                                                                                                                                                          
   

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    We have a custom Zynq board with Micrel KSZ9031RNX phy. And we get sometimes "xemacps e000b000.eth: transmit timeout 3000 ms" error message but could not find the solution yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • linux.matthew
    0 linux.matthew over 13 years ago

    I'm having a similar problem with my Avnet zedboard where the ethernet seems to flake out capriciously with the following error:

    xemacps e000b000.ps7-ethernet: transmit timeout 3000 ms, reseting...
    xemacps e000b000.ps7-ethernet: Set clk to 124999998 Hz
    xemacps e000b000.ps7-ethernet: link up (1000/FULL)

    This is really getting annoying.

    Matt