Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Ampere Hour Meter for Tango Control System with Zynq, XADC, AMP, OCM
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 362 subscribers
  • Views 203 views
  • Users 0 members are here
Related

Ampere Hour Meter for Tango Control System with Zynq, XADC, AMP, OCM

e14 Contributor
e14 Contributor over 10 years ago

Dear all,

we registered again a team from the class "Lpro Systèmes embarqués" UJF Grenoble in the Xilinx University Contest, OpenHardware 2016 (http://www.openhw.eu/)


This app use Assymetric Multiprocessor : one ARM core for linux/tango device server and the other one for a standalone bare metal app (human safety can't rely on a non deterministic linux app). Communication use OnChipMemory. Linux is custom OpenEmbedded. We use Zynq internal XADC to monitor the current in Transfer Line between Booster and Storage Ring, this current is an image of the radiation dose.

youtube : youtu.be/J34uoM3a1pM

paper : https://docs.google.com/document/d/1glvFaKJogfreaWkISOiwTDw1JLJJtfZDZQDQ5kmIFsI

Tango Distributed Control System : www.tango-controls.org
ESRF : www.esrf.eu

try it ! download files : 
zedboard SD : http://dl.free.fr/huOxTA DZV
virtualbox tango/ubuntu image : http://www.tango-controls.org/downloads/virtual-machine/

Tango is a free, open source, scalable, efficient SCADA framework : a set of tools and API to monitor industrial appliance of any kinds... 
Tango control system was elaborated at the ESRF, a large synchrotron radiation facility in Grenoble, France. The ESRF is a large research laboratory (1500 engineers, researchers, ), a kind of giant microscope to explore organic molecules or others and that uses X rays of high energy (6 GeV) issued from an 850 meters circumference accelerator in more than 40 beams lines operating simultaneously.

Tango Control System is a 100 man/years middleware, which aims at the monitoring 24/7 of more than 200 000 sensors & actuators in the facility. It features among other usage : logging, events driven communication, seamless integration to NI Labview, Matlab, Igor scientific toolboxes or OPC-UA plc, EPICS bus, ...