Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development My software doesn't work if optimization is enabled
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 373 views
  • Users 0 members are here
Related

My software doesn't work if optimization is enabled

100prathima
100prathima over 10 years ago

Hi:
I am currently working on an embedded software with hard real time constraints. My ISR should execute every milli second. I have a working software version(standalone) which I need to optimize. If I simply enable -o2 or -o3, the software doesn't work as before. So, how do I use these optimization options in a real time system? Am I missing anything? 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Software optimization using compiler settings is usually pretty safe, but if you are using code such as that typically found in an ISR, you may have variables that are changed outside the current execution context.  Since the compiler may not be aware of this, optimizing the code can result in removal of "extraneous" variables (which are actually critical) or the reordering of code to "optimize" pipeline operations (which in some cases inadvertently changes a critical flow sequence) causing an incorrect result.

    So in the vast majority of cases you can solve the problem by using #pragmas to control the level of GCC optimization, or declaring variables as volatile so the compiler doesn't optimize them out when it shouldn't.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100prathima
    0 100prathima over 10 years ago in reply to e14 Contributor

    I was enabling the project optimization and it was not working. If I select optimization for required files, the code works and there seems to be improvement. So, what is the difference between file level optimization and optimization for entire project?