Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Carrier card V2 default frequencies
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 362 subscribers
  • Views 312 views
  • Users 0 members are here
Related

Carrier card V2 default frequencies

halc
halc over 9 years ago

Hey all,

I am currently starting developing on the picozed with carrier card v2. There is the IDT 8T49N242-006 clock synthesizer IC which provides the MGT and PL clock for the Zynq.

Does anybody knows the default frequencies of Q2 and Q3 output of the IC?

 

BR

Chris

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 9 years ago

    Hi there,

    From the factory, the clock is not set.  You will need to use "Transceiver Clock Programming Reference Design" in order to setup the clock.  There are 3 examples included. 

        *MUX in a clock from the PCIe card edge
        *MUX in a clock from the FMC connector
        *The "default" configuration used in all the provided reference designs, 250MHz.

    There is a set of these for each of the PicoZed transceiver based SOMs (PZ7015/PZ7030).  Each of these files are bootable BIN files that you can use to directly program the part without needing to run the entire reference design.  I would suggest you follow the instructions provided in the design to properly configure the card for SDCARD boot as well as validate that the programming is a success!  You can also customize the design with your OWN frequencies!

    If you use the 250MHz BIN file, the chip is configured for a 250MHz clock on both Q3 and Q4.

    You can locate the reference design here:
    http://picozed.org/support/design/13076/106

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 9 years ago

    Hi there,

    From the factory, the clock is not set.  You will need to use "Transceiver Clock Programming Reference Design" in order to setup the clock.  There are 3 examples included. 

        *MUX in a clock from the PCIe card edge
        *MUX in a clock from the FMC connector
        *The "default" configuration used in all the provided reference designs, 250MHz.

    There is a set of these for each of the PicoZed transceiver based SOMs (PZ7015/PZ7030).  Each of these files are bootable BIN files that you can use to directly program the part without needing to run the entire reference design.  I would suggest you follow the instructions provided in the design to properly configure the card for SDCARD boot as well as validate that the programming is a success!  You can also customize the design with your OWN frequencies!

    If you use the 250MHz BIN file, the chip is configured for a 250MHz clock on both Q3 and Q4.

    You can locate the reference design here:
    http://picozed.org/support/design/13076/106

    --Dan