Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development hello world
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 446 views
  • Users 0 members are here
Related

hello world

e14 Contributor
e14 Contributor over 14 years ago

Hello all
I try to run the hello world application on the zedboard according the tutorial "..Concepts, Tools and Technics.."but when i start run (page 24) I get the following error message:

14:09:20 INFO  : Processing command line option -hwspec I:/zedboard/Versuch1/project_1/project_1.sdk/SDK/SDK_Export/hw/system.xml.
14:12:46 INFO  : Running ps7 initialization as the processor is not initialized
14:12:46 INFO  : Initializing ps7....
14:12:55 INFO  : ps7 initialization is done.
14:12:56 ERROR : Unexpected error while launching program. java.lang.RuntimeException:
tat com.xilinx.sdk.targetmanager.internal.TM.verifyELF(Unknown Source)
tat com.xilinx.sdk.debug.core.internal.AppRunner.run(Unknown Source)
Any help available?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I use 14.1 and 14.2.
    The mentiond error disappeard when I imported the correct zedboard definition file and the first part of hello world application worked.
    I then started the extended version of hello word (with timer and axi gpio and chipscope). Here I have again proplems. Under planahead and XPS 14.1 I cannot make any compilation because I get the message "no license for chipscope". Under planahead and XPS 14.2 I get the hardware compiled and bitstream is generated. But the SDK now complains about missing xgpio.h and xtmrctr.h and I don't know what I am doing wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    which definition file did you used?
    i have the same problem i used "zedboard_RevC_v2.xml"
    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I finished the tutorial properly, but when I changed the Text, which should be displayed,  into the German "Hallo Welt" still "Hello World" is printed into the console. How could this happen, if the code has changed?? I tried to clean up project, but it doesn't work anyway:(