Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Mapping linux driver to GPIO
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 1412 views
  • Users 0 members are here
Related

Mapping linux driver to GPIO

e14 Contributor
e14 Contributor over 10 years ago

Hi All,

I have currently mapped two GPIO to be used with slave devices to operate with I2C. I also have checked the mapped GPIO by writing 1/0 through command like and checking the signal through an oscilloscope.

I would like to map the I2C driver already there in the kernel to be used with these two GPIO pins.

Question:

1. How do I map the linux kernel I2C driver to GPIO so that I can communicate with the slave devices.

2. There are 4 i2c commands: i2cdetect, i2cdump, i2cget, i2cset. Is there any documentation on how to use them?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 10 years ago

    Hi yathindra,

    Using the I2C driver is going to make your life a lot easier since the interface details of I2C get abstracted way by this driver making it much simpler to write your user space application.  You won't need to perform MMAP operation and hassle with the timing of GPIO to implement I2C if you simply use one of the I2C controllers (either PS I2C or PL AXI IIC) and the corresponding driver.

    We have an example of how to use PL I2C from Linux and you can download this "Wind River Pulsar Linux OS with I2C Peripheral Integration" tutorial from the reference designs page:

    http://microzed.org/support/design/13591/116

    This will involve making sure that the appropriate I2C driver is built into the kernel, there is a valid device tree entry for the I2C controller instance, and that the userspace application is accessing the I2C driver correctly.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 10 years ago

    Hi yathindra,

    Using the I2C driver is going to make your life a lot easier since the interface details of I2C get abstracted way by this driver making it much simpler to write your user space application.  You won't need to perform MMAP operation and hassle with the timing of GPIO to implement I2C if you simply use one of the I2C controllers (either PS I2C or PL AXI IIC) and the corresponding driver.

    We have an example of how to use PL I2C from Linux and you can download this "Wind River Pulsar Linux OS with I2C Peripheral Integration" tutorial from the reference designs page:

    http://microzed.org/support/design/13591/116

    This will involve making sure that the appropriate I2C driver is built into the kernel, there is a valid device tree entry for the I2C controller instance, and that the userspace application is accessing the I2C driver correctly.

    Regards,

    -Kevin