Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Mapping linux driver to GPIO
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 1412 views
  • Users 0 members are here
Related

Mapping linux driver to GPIO

e14 Contributor
e14 Contributor over 10 years ago

Hi All,

I have currently mapped two GPIO to be used with slave devices to operate with I2C. I also have checked the mapped GPIO by writing 1/0 through command like and checking the signal through an oscilloscope.

I would like to map the I2C driver already there in the kernel to be used with these two GPIO pins.

Question:

1. How do I map the linux kernel I2C driver to GPIO so that I can communicate with the slave devices.

2. There are 4 i2c commands: i2cdetect, i2cdump, i2cget, i2cset. Is there any documentation on how to use them?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    I was able to read/write from the external device (EEPROM connected with I2C) using the Xilinx driver  http://www.wiki.xilinx.com/Linux+I2C+Driver , however I have the following two questions, 

    1. Is the driver specific to EEPROM alone?  I would like to know if the same can be used with other I2C devices like a DAC, LCD etc? I cannot actually test other devices for a few days until I get the devices though. 

    2. This driver does read and write, is there any easy way to probe for I2C devices as well?

    Currently I am checking /sys/class/i2c/ for the devices present and including them in the driver code..

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    I was able to read/write from the external device (EEPROM connected with I2C) using the Xilinx driver  http://www.wiki.xilinx.com/Linux+I2C+Driver , however I have the following two questions, 

    1. Is the driver specific to EEPROM alone?  I would like to know if the same can be used with other I2C devices like a DAC, LCD etc? I cannot actually test other devices for a few days until I get the devices though. 

    2. This driver does read and write, is there any easy way to probe for I2C devices as well?

    Currently I am checking /sys/class/i2c/ for the devices present and including them in the driver code..

    Thanks