Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development standalone application command line flow
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 297 views
  • Users 0 members are here
Related

standalone application command line flow

e14 Contributor
e14 Contributor over 12 years ago

Hi,
I wonder if you can explain to me what is going on when I try and run a program on the zedboard.

The scenario that works is (from board power up):

1.tLaunch the SDK from Vivado.
2.tProgram the FPGA.
3.tRun a program (using the Xilinx C/C++ application (GDB)) that accesses a few memory mapped registers in the PL.
4.tNow launch another program from the command line using xmd:
source proc/hw_platform_0/ps7_init.tcl
connect arm hw
ps7_init
fpga -f output/arm_subsystem_wrapper.bit
rst -processor
dow proc/test/Debug/test.elf
run

This all works fine.

The scenario that doesnu2019t work is (from board power up):
1.tUse xmd to run a program from the command line using xmd:
source proc/hw_platform_0/ps7_init.tcl
connect arm hw
ps7_init
fpga -f output/arm_subsystem_wrapper.bit
rst -processor
dow proc/test/Debug/test.elf
run

This doesnu2019t work.  Itu2019s as if the SDK is running something else too other than just the application elf file that does some start-of day configuration stuff.  I am running a baremetal application (using the helloworld example target).  If I take out the FPGA register reads the second scenario works (essentially just doing print(u201CHello World
ru201D);)

Any ideas?  I think to have a viable Zynq flow we really need a way of building and launching from the command line without having to involve the SDK.

Regards,
Scott

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    In case anyone else runs into this, I posted the same query on the xilinx forums and got a solution:

    http://forums.xilinx.com/t5/Zynq-All-Programmable-SoC/standalone-application-command-line-flow/m-p/400155/highlight/false#M1003