Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PCIe issue with Pulsar Linux on the Zynq Mini-ITX
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 362 subscribers
  • Views 448 views
  • Users 0 members are here
Related

PCIe issue with Pulsar Linux on the Zynq Mini-ITX

e14 Contributor
e14 Contributor over 10 years ago

PCIe support has been inadvertently omitted in the configuration present for the Pulsar7 release for the Zynq Mini-ITX.  If you want to use PCIe cards with this motherboard, please follow this procedure:

Download and install the free wr-core toolchain from Wind River Open Source Labs:

http://www.windriver.com/products/linux/open-source-leadership

Follow the instructions on the Github site to install the toolchain and Linux source on a Linux host.  Don’t follow the build instructions yet.

First edit:

<install-dir>/wr-core/layers/wrlabs-integration/recipes-kernel/linux/files/xilinx-zynq.cfg

 

Add these lines to the configuration file to activate PCIe in the kernel:

CONFIG_PCI=y

CONFIG_PCI_SYSCALL=y

CONFIG_PCI_MSI=y

# CONFIG_PCI_DEBUG is not set

CONFIG_PCI_REALLOC_ENABLE_AUTO=y

# CONFIG_PCI_STUB is not set

CONFIG_PCI_ATS=y

CONFIG_PCI_IOV=y

CONFIG_PCI_PRI=y

CONFIG_PCI_PASID=y

### The PCI bridge

CONFIG_PCIE_XILINX=y

 

Save the xilinx-zynq.cfg file. 

Check out the Pulsar 7 branch.

cd wr-core

git pull

git checkout pulsar-7.0

git submodule update --init

 

Now follow the build instructions on the Github site for the Zynq Mini-ITX board.   This will provide an image file that you can then write to an 8 GB uSD card.

Boot the board from the new image, and PCIe should be active.  You can plug in a PCIe card and probe the bus with:   lspci –m