Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Booting up with larger image
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 493 views
  • Users 0 members are here
Related

Booting up with larger image

e14 Contributor
e14 Contributor over 13 years ago

I have increased the size of the .image file included in the out of box package as the original did not have much room to install programs. Now I am having issues while attempting to boot. What further steps would I have to take? Below is the terminal output:

In:    serial
Out:   serial
Err:   serial
Net:   zynq_gem
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Device: SDHCI
Manufacturer ID: 3
OEM: 5344
Name: SU04G
Tran Speed: 25000000
Rd Block Len: 512
SD version 1.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
reading zImage

2479640 bytes read
reading devicetree_ramdisk.dtb

5817 bytes read
reading ramdisk8M.image.gz

4724910 bytes read
## Starting application at 0x00008000 ...
Uncompressing Linux... done, booting the kernel.
[    0.000000] Booting Linux on physical CPU 0
[    0.000000] Linux version 3.3.0-digilent-12.07-zed-beta (tinghui.wang@DIGILENT_LINUX) (gcc version 4.6.1 (Sourcery CodeBench Lite 2011.09-50) ) #2 SMP PREEMPT Thu Jul 12 21:01:42 PDT 2012
[    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZED
[    0.000000] bootconsole [earlycon0] enabled
[    0.000000] Memory policy: ECC disabled, Data cache writealloc
[    0.000000] BUG: mapping for 0xf8f00000 at 0xfe00c000 out of vmalloc space
[    0.000000] BUG: mapping for 0xe0000000 at 0xfe000000 out of vmalloc space
[    0.000000] BUG: mapping for 0xffff1000 at 0xfe200000 out of vmalloc space
[    0.000000] PERCPU: Embedded 7 pages/cpu @c1489000 s5696 r8192 d14784 u32768
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 125824
[    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/ram rw initrd=0x800000,8M earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=0
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 240MB 256MB = 496MB total
[    0.000000] Memory: 489856k/489856k available, 34432k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xfd000000   ( 456 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc042f040   (4253 kB)
[    0.000000]       .init : 0xc0430000 - 0xc0456640   ( 154 kB)
[    0.000000]       .data : 0xc0458000 - 0xc0485dc0   ( 184 kB)
[    0.000000]        .bss : 0xc0485de4 - 0xc049d734   (  95 kB)
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Verbose stalled-CPUs detection is disabled.
[    0.000000] NR_IRQS:128
[    0.000000] xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43
[    0.000000] Console: colour dummy device 80x30
[    0.000000] Calibrating delay loop... 1594.16 BogoMIPS (lpj=7970816)
[    0.090000] pid_max: default: 32768 minimum: 301
[    0.090000] Mount-cache hash table entries: 512
[    0.090000] CPU: Testing write buffer coherency: ok
[    0.090000] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.100000] smp_twd: clock not found: -2
[    0.100000] Calibrating local timer... 399.37MHz.
[    0.170000] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[    0.170000] Setting up static identity map for 0x2f8d48 - 0x2f8d7c
[    0.270000] CPU1: Booted secondary processor
[    0.310000] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.310000] Brought up 2 CPUs
[    0.310000] SMP: Total of 2 processors activated (3188.32 BogoMIPS).
[    0.320000] devtmpfs: initialized
[    0.320000] ------------[ cut here ]------------
[    0.320000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()
[    0.330000] Modules linked in:
[    0.330000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4c/0x64)
[    0.340000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+0x18/0x1c)
[    0.350000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/0x104)
[    0.360000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x160)
[    0.360000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)
[    0.370000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)
[    0.380000] ---[ end trace 1b75b31a2719ed1c ]---
[    0.380000] ------------[ cut here ]------------
[    0.390000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()
[    0.390000] Modules linked in:
[    0.390000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4c/0x64)
[    0.400000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+0x18/0x1c)
[    0.410000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/0x104)
[    0.420000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x160)
[    0.430000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)
[    0.430000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)
[    0.440000] ---[ end trace 1b75b31a2719ed1d ]---
[    0.440000] NET: Registered protocol family 16
[    0.460000] L310 cache controller enabled
[    0.460000] l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72060000, Cache size: 524288 B
[    0.460000] registering platform device 'pl330' id 0
[    0.470000] registering platform device 'arm-pmu' id 0
[    0.470000]
[    0.470000] ###############################################
[    0.480000] #                                             #
[    0.480000] #                Board ZED Init               #
[    0.480000] #                                             #
[    0.490000] ###############################################
[    0.490000]
[    0.500000] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.500000] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.530000] xslcr xslcr.0: at 0xF8000000 mapped to 0xE0808000
[    0.540000] bio: create slab <bio-0> at 0
[    0.540000] gpiochip_add: registered GPIOs 0 to 245 on device: xgpiops
[    0.540000] xgpiops e000a000.gpio: gpio at 0xe000a000 mapped to 0xe080a000
[    0.550000] SCSI subsystem initialized
[    0.550000] usbcore: registered new interface driver usbfs
[    0.560000] usbcore: registered new interface driver hub
[    0.560000] usbcore: registered new device driver usb
[    0.570000] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.570000] Switching to clocksource xttcpss_timer1
[    0.580000] NET: Registered protocol family 2
[    0.580000] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[    0.580000] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[    0.590000] TCP bind hash table entries: 16384 (order: 5, 196608 bytes)
[    0.590000] TCP: Hash tables configured (established 16384 bind 16384)
[    0.600000] TCP reno registered
[    0.600000] UDP hash table entries: 256 (order: 1, 8192 bytes)
[    0.610000] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[    0.610000] NET: Registered protocol family 1
[    0.620000] Trying to unpack rootfs image as initramfs...
[    0.620000] rootfs image is not initramfs (no cpio magic); looks like an initrd
[    0.650000] Freeing initrd memory: 8192K
[    0.660000] xscugtimer xscugtimer.0: ioremap fe00c200 to e0810200 with size 400
[    0.660000] pl330 dev 0 probe success
[    0.670000] msgmni has been set to 972
[    0.670000] io scheduler noop registered
[    0.670000] io scheduler deadline registered
[    0.670000] io scheduler cfq registered (default)
[    0.680000] e00   0.680000] console [ttyPS0] enabled, bootconsole disabled
[    0.680000] console [ttyPS0] enabled, bootconsole disabled
[    0.690000] xdevcfg f8007000.devcfg: ioremap f8007000 to e0814000 with size 1000
[    0.700000] [drm] Initialized drm 1.1.0 20060810
[    0.710000] brd: module loaded
[    0.720000] loop: module loaded
[    0.720000] xqspips e000d000.qspi: at 0xE000D000 mapped to 0xE0816000, irq=51
[    0.730000] GEM: BASEADDRESS hw: e000b000 virt: e0818000
[    0.730000] XEMACPS mii bus: probed
[    0.740000] eth0, pdev->id -1, baseaddr 0xe000b000, irq 54
[    0.740000] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    0.750000] usb_hcd_xusbps_probe: No OTG assigned!
[    0.750000] usb_hcd_xusbps_probe: OTG now assigned!
[    0.750000] xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
[    0.760000] xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
[    0.800000] xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
[    0.820000] xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
[    0.820000] hub 1-0:1.0: USB hub found
[    0.820000] hub 1-0:1.0: 1 port detected
[    0.830000] Initializing USB Mass Storage driver...
[    0.830000] usbcore: registered new interface driver usb-storage
[    0.840000] USB Mass Storage support registered.
[    0.840000] Xilinx PS USB Device Controller driver (Apr 01, 2011)
[    0.850000] mousedev: PS/2 mouse device common for all mice
[    0.850000] Linux video capture interface: v2.00
[    0.860000] gspca_main: v2.14.0 registered
[    0.860000] usbcore: registered new interface driver uvcvideo
[    0.860000] USB Video Class driver (1.1.1)
[    0.870000] WDT OF probe
[    0.870000] xwdtps f8005000.swdt: Xilinx Watchdog Timer at 0xe081c000 with timeout 10 seconds
[    0.880000] sdhci: Secure Digital Host Controller Interface driver
[    0.880000] sdhci: Copyright(c) Pierre Ossman
[    0.890000] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.890000] mmc0: Invalid maximum block size, assuming 512 bytes
[    0.900000] No connectors reported connected with modes
[    0.900000] [drm] Cannot find any crtc or sizes - going 1024x768
[    0.910000] mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
[    0.910000] usbcore: registered new interface driver usbhid
[    0.920000] drivers/gpu/drm/analog/analog_drm_fbdev.c:analog_drm_fbdev_probe[241]
[    0.930000] usbhid: USB HID core driver
[    0.930000] adv7511 0-0039: Failed to add route DAI IN->TMDS
[    0.960000] Console: switching to colour frame buffer device 128x48
[    0.970000] asoc: adv7511 <-> 75c00000.axi-spdif-tx mapping ok
[    0.970000] axi-spdif 75c00000.axi-spdif-tx: Failed to set DAI format: -22
[    0.990000] fb0:  frame buffer device
[    0.990000] drm: registered panic notifier
[    1.000000] [drm] Initialized analog_drm 1.0.0 20110530 on minor 0
[    1.000000] ALSA device list:
[    1.000000]   #0: HDMI monitor
[    1.010000] TCP cubic registered
[    1.010000] NET: Registered protocol family 17
[    1.010000] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    1.020000] Registering SWP/SWPB emulation handler
[    1.030000] registered taskstats version 1
[    1.030000] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
[    1.030000] RAMDISK: gzip image found at block 0
[    1.070000] mmc0: new high speed SDHC card at address e624
[    1.080000] mmcblk0: mmc0:e624 SU04G 3.69 GiB
[    1.080000]  mmcblk0: p1
[    1.390000] RAMDISK: incomplete write (31278 != 32768)
[    1.400000] write error
[    1.550000] EXT4-fs (ram0): bad geometry: block count 1025024 exceeds size of device (35384 blocks)
[    1.610000] List of all partitions:
[    1.610000] b300         3872256 mmcblk0  driver: mmcblk
[    1.610000]   b301         3868160 mmcblk0p1 00000000-0000-0000-0000-000000000mmcblk0p1
[    1.620000] No filesystem could mount root, tried:  ext4
[    1.620000] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)
[    1.630000] CPU1: stopping
[    1.630000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c0011c10>] (handle_IPI+0xf4/0x164)
[    1.640000] [<c0011c10>] (handle_IPI+0xf4/0x164) from [<c00084c0>] (gic_handle_irq+0x90/0x9c)
[    1.650000] [<c00084c0>] (gic_handle_irq+0x90/0x9c) from [<c000d240>] (__irq_svc+0x40/0x70)
[    1.650000] Exception stack(0xd8067fa0 to 0xd8067fe8)
[    1.660000] 7fa0: d8066000 d8066028 d8067fe8 00000000 c0463768 00000015 10c0387d c0486160
[    1.660000] 7fc0: 0000406a 413fc090 00000000 00000000 00000000 d8067fe8 c000e02c c000e030
[    1.670000] 7fe0: 60000013 ffffffff
[    1.670000] [<c000d240>] (__irq_svc+0x40/0x70) from [<c000e030>] (default_idle+0x24/0x28)
[    1.680000] [<c000e030>] (default_idle+0x24/0x28) from [<c000e1d8>] (cpu_idle+0x38/0x9c)
[    1.690000] [<c000e1d8>] (cpu_idle+0x38/0x9c) from [<00449b14>] (0x449b14)
[    1.690000] panic occurred, switching back to text console
[    1.700000] [drm:drm_crtc_helper_set_config],
[    1.700000] [drm:drm_crtc_helper_set_config], [CRTC:3] [NOFB]

It appears I have a 35 MB limit by reading through this, is there any way I can access the rest of the SD card?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Yes I am still using the default one, I'll keep that in mind. However my issues isn't in creating the image but I believe it is in the BOOT.bin or something dealing with uboot. The reason being I had a similar issue when switching from the image that came on the sd card to the newer "out of box" one from this website. It didn't work when I copied over just the .gz file, however when I switched over the bin and other files it did. I am currently attempting things listed here: http://www.zedboard.org/content/recompile-linux-kernel as it seems like a possible solution but I am unsure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Up until 1.08 it looks normal so I belive the issue starts with [ 1.390000] RAMDISK: incomplete write (31278 != 32768)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Up until 1.08 it looks normal so I belive the issue starts with [ 1.390000] RAMDISK: incomplete write (31278 != 32768)