Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Possible to develop application  on Zedboard and deploy on PicoZed ?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 630 views
  • Users 0 members are here
Related

Possible to develop application  on Zedboard and deploy on PicoZed ?

e14 Contributor
e14 Contributor over 10 years ago

I have to develop an C++ application which shall run on the PicoZed 7015 SOM.

For development, I would prefer to compile the application  on the Zedboard devlopment board.
As is noted in http://microzed.org/content/xillinux-run-ubuntu-linux-desktop-zedboard  , it seems to be possible to use the Zedboard directly as a computer (with keyboard, monitor and mouse) with a ubuntu-like desktop. So i should be able to use the usual tools (cmake, gcc, ..) to compile my C++ application and all libraries (like OpenCV).


My question is now - can I run the binaries, which I have compiled on the Zedboard, directly on the PicoZed?



  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Ok, that sounds positive, but I have some questions:

    @Bryan:
    * What do you mean with a 'bitstream change' ?
    * What is a 'address map', and how can I change it ?

    @Ron:
    * I would prefer to use 'Xillinux' for compiling the application and not 'PetaLinux', because - as mentioned in the link I gave - i can develop in the 'usual way' with cmake, gcc, and a operating system with a GUI. Is that possible, or do I _have_ to use 'PetaLinux' for building the binaries ?

    Maybe I should note that my application will _not_ use the FPGA or other peripherials, its algorithms will run only on the ARM Cortex A9 CPU.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Ok, that sounds positive, but I have some questions:

    @Bryan:
    * What do you mean with a 'bitstream change' ?
    * What is a 'address map', and how can I change it ?

    @Ron:
    * I would prefer to use 'Xillinux' for compiling the application and not 'PetaLinux', because - as mentioned in the link I gave - i can develop in the 'usual way' with cmake, gcc, and a operating system with a GUI. Is that possible, or do I _have_ to use 'PetaLinux' for building the binaries ?

    Maybe I should note that my application will _not_ use the FPGA or other peripherials, its algorithms will run only on the ARM Cortex A9 CPU.