Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development XAPP1078 - Recompile kernel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 608 views
  • Users 0 members are here
Related

XAPP1078 - Recompile kernel

e14 Contributor
e14 Contributor over 12 years ago

Hi !


I am trying to run the XAPP1078 (Linux on CPU0, Bare-metal app on CPU1) on my MicroZed.


I have succesfully ran your ZedBoard adaptation (http://zedboard.org/sites/default/files/design/xapp1078_zedboard.zip) with the prebuilt linux kernel that is given in the zip. However, I am unable to do it when I compile my own kernel.


When using my kernel, the CPU1 won't start. If I connect a JTAG debugger, I can see it's PC is at 0x00000004. If I manually set the PC to 0x18000000, the Linux kernel will panic soon after.

My guess is that the provided kernel isn't built from clean sources as the XAPP1078 pdf says.

The same reasonning applies to U-Boot :
* The XAPP1078 pdf and the "Simple_AMP_Zedboard.pdf" both stand that U-Boot is compiled from unpatched Xilinx sources.
* The precompiled U-Boot uses less than total available memory to avoid erasing the CPU1 elf.
* If I compile U-Boot from Xilinx sources, it will uses the entire memory.
=> Something's wrong...


Thanks for your help,


Julien.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Julien,

    I'm not sure what your issue is, I've not been able to do a working build for XAPP1078 either, but some here's some info that might help:
    http://www.wiki.xilinx.com/XAPP1078+Latest+Information

    In xapp1078_zedboard.zip there is a Readme2.txt file in the design folder that describes the steps taken to modify the sources for the zedboard.

    u-boot has two environment variables that may be relevant:
    initrd_high=0x20000000
    fdt_high=0x20000000

    Also there a few other threads here about XAPP1078 and on the Xilinx forum that might help, e.g.
    http://www.zedboard.org/content/amp-running-linux-and-bare-metal-system-both-zynq-soc-processors

    Best regards, Sam.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Julien,

    I'm not sure what your issue is, I've not been able to do a working build for XAPP1078 either, but some here's some info that might help:
    http://www.wiki.xilinx.com/XAPP1078+Latest+Information

    In xapp1078_zedboard.zip there is a Readme2.txt file in the design folder that describes the steps taken to modify the sources for the zedboard.

    u-boot has two environment variables that may be relevant:
    initrd_high=0x20000000
    fdt_high=0x20000000

    Also there a few other threads here about XAPP1078 and on the Xilinx forum that might help, e.g.
    http://www.zedboard.org/content/amp-running-linux-and-bare-metal-system-both-zynq-soc-processors

    Best regards, Sam.