Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development add custom constraints to HDL coder
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 820 views
  • Users 0 members are here
Related

add custom constraints to HDL coder

100stefanoo
100stefanoo over 8 years ago

My Simulink project is now progressing steadily!

Compatibility for the Digilent AD2 PMOD peripheral is now working but my programming procedure make use of a trick which I would like to avoid.

Because I need to add constraints for internal pullups I tipically stop the workflow after RTL generation, include the constraints in the .xdc file automatically generated and then proceed with the bitstream generation.

I do this ugly thing because Simulink doesn't seem to offer the possibility to add PULLUP constraints to the system port.

 
Then i saw in the MiniZed compatibility package an .xdc file for the wifi pins.
Could I add my constraints to this file and expect to be picked-up at each generation?
Is there a truly elegant way of doing this?
  • Sign in to reply
  • Cancel
  • mbrown
    0 mbrown over 8 years ago

    Glad to hear you're making progress!

    You can add custom constraints in two ways:

    1) Add them to the .xdc you found in the MiniZed add-on folder (your current method):

    C:\Users\<user>\Documents\MATLAB\Add-Ons\Toolboxes\Avnet MiniZed Support Package for Simulink\code\hdlcoder\MiniZed\+MiniZedRegistration\+Vivado2017_2\minized_wifi_pins.xdc

     

    2) You should also be able to add an additional .xdc constraints file for HDL Workflow Advisor. Just add it to

    C:\Users\<user>\Documents\MATLAB\Add-Ons\Toolboxes\Avnet MiniZed Support Package for Simulink\code\hdlcoder\MiniZed\+MiniZedRegistration\+Vivado2017_2\plug_rd.m

    % Add custom Vivado constraints
    hRD.CustomConstraints = {'minized_wifi_pins.xdc', 'PMOD_pins.xdc'};

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • 100stefanoo
    0 100stefanoo over 8 years ago in reply to mbrown

    adding to the list in plugin_rd.m is great! thanks!!!