Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Data Aquisition  on ZYNQ board via PMOD I/Os
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 266 views
  • Users 0 members are here
Related

Data Aquisition  on ZYNQ board via PMOD I/Os

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I am working on a project which revolves arround Ultrasonic and IR Sensors. I have arduino board that is triggering one of the sensors and getting data from IR and further sending it to its Serial out pins (Tx and Rx).

On the other end I want a Ultrasonic Module to be interfaced with zynq via PMOD IOs and this time, zynq Ps will trigger it using PWM.

I need suggestions in Which type of communication (SPI or UART or any other) I would need to input the data via PMOD from arduino's Serial pins.

Also since I am new to PMODs. Could some one share a tutorial on basic working of PMOD and data fetching to Zynq PS via PMOD where a hardware on PL and software driver is implemented.

I need more than one PMODs, as far as I have seen there is only one JE1 connected directly to PS. For others we have to describe in HDL.

Any Suggestion and Help, link to example application note or tutorial will be helpful.

I will further develop the algorithm on PS on the basis of sensor values.

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 12 years ago

    The Maxim Analog Essentials provides some examples.

    http://maximintegrated.com/pmod

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 12 years ago

    The Maxim Analog Essentials provides some examples.

    http://maximintegrated.com/pmod

     

    Bryan