Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Bring Ti WiLink 8 to Petalinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 658 views
  • Users 0 members are here
Related

Bring Ti WiLink 8 to Petalinux

hai.bi
hai.bi over 11 years ago

The image from Yocto works fine but I need instructions on how to step by step build a petalinux image that can enable the wi-Fi from TI WiLink 8 module.

I have following problems:

1. In Vivado, how do I set the  direction of MIO 0?
2. What should be there in the system-top.dts ?
3. any more steps need to connect the SDIO to the Wi-Fi module?


Regards,

  • Sign in to reply
  • Cancel
  • peterfenn
    0 peterfenn over 11 years ago

    As you found-out, newer versions of Vivado do not allow MIO pins to be set to IN or OUT (these pins instead a static INOUT type)

    Setting u201Cbroken-cdu201D in the DTS entry for the SDIO is a better solution as then no connection is required for the CD signal.

    What version Linux Kernel are you using?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hai.bi
    0 hai.bi over 11 years ago in reply to peterfenn

    Xilinx Linux 3.17 is the one I am using. Glad to know MIO will be just INOUT.  What else do I need to do to make TI wifi work?  Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hai.bi
    0 hai.bi over 11 years ago in reply to peterfenn

    How does Zynq know which SDIO controller to use for the wifi? I didn't such information in the device tree or config.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hai.bi
    0 hai.bi over 11 years ago

    I have copied the device tree and SDIO1 is now available as mmc1 (address 0001).  So in order to try the Wi-Fi, I compiled the kernel with loadable modules.  I copied the /lib/firmware directory to the SD card.


    so I can modprobe wlcore, wl18xx separately.  Then I sue modprobe wlcore_sdio.ko, and it complains that wl1271_sdio mmc1:0001:2: missing platform data: -19

    While the Yocto image will say
    wl18xx_driver wl18xx.0.auto: direct firmware load failed with error -2

    How to force wlcore_sdio to use wl18xx instead of looking for wl1271?


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • peterfenn
    0 peterfenn over 11 years ago

    I suggest download the script files provided (for the build with latest ArchiTech SDK) The SDK 2.1.0 Yocto build includes Wilink8 R8.5 driver support and has been verified with kernel 3.17